SRAM Usage and Address Ranges on STM32MP25x in OpenSTLinux
I'm using the Yocto-based OpenSTLinux embedded software on a STM32MP25x and I don't understand which portion of the SRAM1/2 is free to use at runtime.
Aside from the first 4kBytes of the SRAM1 reserved for OTP shadow, can the rest be fully used, or is it also reserved ?
Additionally, in chapter 2.4.2 of the reference manual (RM0457), it states that SRAM1/2 can be accessed through the following address ranges [0x0A04 0000, 0x0A08 0000[, [0x0E04 0000, 0x0E08 0000[, [0x2004 0000, 0x2008 0000[ and [0x3004 0000, 0x3008 0000[. Why are there four physical addresses for SRAM ? Should Cortex-A35 and Cortex-M33 use specific regions to communicate with each other ?