Skip to main content
Associate III
July 23, 2025
Question

ST32MP157F-DK2 CM4 project fails on VIRT_UART_Init

  • July 23, 2025
  • 1 reply
  • 262 views

I generated a project from a ioc f

ile that I created. I'm getting this assert error in 

 

smanger_1-1753304496440.png

smanger_0-1753304470608.png

1 reply

Olivier GALLIEN
Technical Moderator
August 8, 2025

Hi @smanger 

 

Please share ecosystem version you are using

 

Olivier 

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
smangerAuthor
Associate III
August 8, 2025

I think this was happening because the M4 project was build with an IOC file that is different from the Starter Image, so the memory regions do align properly. I can flash LEDs with that code, but when I try to use OPENamp, the program crashes.

I didn't realize this at first. So, I think this will go away once I can build and deploy the A7 that is built from my IOC file, That is still my major concern! I still can not do that and my online support case has yielded absolutely nothing. I'm update to update that because I tried another process listed in the forum. And that doesn't work either.

 

https://ols.st.com/s/case/500Ty00000VdCh2IAF/st32mp157fdk2-openstlinux-project-builddeploy-problems