Skip to main content
debugging
Lead
January 15, 2020
Solved

STM32MP1 Configure USB OTG interface as a gadget device in Linux kernel

  • January 15, 2020
  • 1 reply
  • 2301 views

0690X00000Bw0IKQAZ.pngA particular STM32MP1 based board uses the USB OTG interface configured to the cortex A7. Is there any guidance how to configure the kernel so that it will use the USB device port with a gadget driver, so that the host sees it as keyboard, serial port, mouse, audio interface ? For example, as pictured, a snippet of usb otg in the .dts ( high speed). It uses dwc2 as driver for OTG function, How to assign the device descriptor to the otg/usb interface ? Full speed would be fine as well. In the kernel sources there is "legacy" and "function" code.

This topic has been closed for replies.
Best answer by PatrickF

This is currently the case on STM32MP157C-DK2 board with latest starter package, you could put a keyboard or a mouse on the Type-C port which is connected to USB OTG in high-speed.

e.g. console log on mouse plug

[ ...] usb 1-1: new low-speed USB device number 4 using dwc2
[ ...] input: HP HP USB 1000dpi Laser Mouse as /devices/platform/soc/49000000.usb-otg/usb1/1-1/1-1:1.0/0003:03F0:1198.0003/input/input4
[ ...] hid-generic 0003:03F0:1198.0003: input: USB HID v2.00 Mouse [HP HP USB 1000dpi Laser Mouse] on usb-49000000.usb-otg-1/input0
[ ...] hid-generic 0003:03F0:1198.0004: device has no listeners, quitting

please have a look to https://wiki.st.com/stm32mpu/wiki/OTG_device_tree_configuration for DT configuration.

1 reply

PatrickF
PatrickFBest answer
Technical Moderator
January 15, 2020

This is currently the case on STM32MP157C-DK2 board with latest starter package, you could put a keyboard or a mouse on the Type-C port which is connected to USB OTG in high-speed.

e.g. console log on mouse plug

[ ...] usb 1-1: new low-speed USB device number 4 using dwc2
[ ...] input: HP HP USB 1000dpi Laser Mouse as /devices/platform/soc/49000000.usb-otg/usb1/1-1/1-1:1.0/0003:03F0:1198.0003/input/input4
[ ...] hid-generic 0003:03F0:1198.0003: input: USB HID v2.00 Mouse [HP HP USB 1000dpi Laser Mouse] on usb-49000000.usb-otg-1/input0
[ ...] hid-generic 0003:03F0:1198.0004: device has no listeners, quitting

please have a look to https://wiki.st.com/stm32mpu/wiki/OTG_device_tree_configuration for DT configuration.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
debugging
debuggingAuthor
Lead
August 29, 2023

To close this:  fixed this by adding support in the custom  kernel configuration.