STM32MP13 - Jumbo Frames - Constrained MTU size problem
Hi,
I am working on an Azure RTOS project, which requires jumbo frames capability. My current devkit is a MYD-YF13X to utilize 1 gigabit ethernet PHYs.
My goal is to receive 9000-byte packets, but I am not able to receive any bigger than ~2000 bytes.
Packets with size over 2kB are simply being ignored, as they wouldn't be transferred. The eth interrupts and respective receive complete callbacks are not being activated for them.
I performed the following configuration:

I have also configured the YT8521-SH ethernet PHY to work with jumbo frames

I have also adapted the size of the buffers respectively.
At the end I worked with the OpenSTLinux with both STM32MP13-Devkit and MYD-YF13X. I wanted to resize the MTU of eth interface. With the ifconfig tool I wasn't able to set the MTU to 9000 bytes. Once again, it was constrained to 2000 bytes.

Why is the constraint set to ~2000?
I would be thankful for any advice and help.
Best,
J.Schneider