Skip to main content
Associate
November 21, 2025
Question

STM32MP135F clock config issue

  • November 21, 2025
  • 0 replies
  • 330 views

Hello engineers, I'm using the latest version of CubeMX and creating a project with STM32MP135FAFx, but the highest clock configuration I can select is 650MHz. According to the datasheet, the maximum supported clock is 1GHz. Someone else has raised the same issue before 👉🏻https://community.st.com/t5/stm32-mpus-products-and-hardware/stm32mp135f-clock-config/m-p/720882#M11932. My CubeMX version is 6.16.0.

This is my screenshot:

QinWei_0-1763686992581.png

This is a screenshot I saw online of someone else configuring their computer to 1GHz, and I'm quite certain that someone else has configured their computer to 1GHz like this before.

dac02f9292167c1d96d8dce5a4b0d85a.png

Could the engineers please help me determine if the problem lies with my usage or with CubeMX itself?

Thank you!