Skip to main content
Associate
February 28, 2024
Solved

Stm32mp15 bootcount environment variable being overwritten in environment

  • February 28, 2024
  • 2 replies
  • 1968 views

Im attempting to set up A/B partitioning on an STM32MP157d-dk1 board so that it can switch between partitions when updating. The board image is built using yocto, and I have used the meta-st-stm32mp layer, and am building a modified version of core-image-full-cmdline for the image.

I have set up fw_setenv and fw_printenv using the following fw_env.config file:

# Configuration file for fw_(printenv/setenv) utility.
# Up to two entries are valid, in this case the redundant
# environment sector is assumed present.
# Notice, that the "Number of sectors" is not required on NOR and SPI-dataflash.
# Futhermore, if the Flash sector size is omitted, this value is assumed to
# be the same as the Environment size, which is valid for NOR and SPI-dataflash
# Device offset must be prefixed with 0x to be parsed as a hexadecimal value.

# On a block device a negative offset is treated as a backwards offset from the
# end of the device/partition, rather than a forwards offset from the start.

# Block device example
/dev/mmcblk0p3 -0x2000 0x2000
/dev/mmcblk0p3 -0x4000 0x2000

 This gives me access to the u-boot environment, and I can modify the bootlimit and upgrade_available variables without issue. However, bootcount is always overwritten on a reboot with its old value incremented by one, and it is incremented regardless of whether upgrade_available is set.

I have enabled bootcount in the uboot settings and have CONFIG_BOOTCOUNT_GENERIC=y set in the defconfig.

I am guessing one of two things is happening:

The bootcount variable is being altered by some other script within the image, in which case I will need some way to find what is modifying it

Or

The bootcount variable is stored elsewhere and is applied to the uboot environment on boot, in which case I need to find this location.

I have checked the U-boot configuration and found the following options for the U-boot environment:

CONFIG_ENV_OFFSET=0x480000
CONFIG_ENV_SECT_SIZE=0x40000
CONFIG_ENV_OFFSET_REDUND=0x4C0000
CONFIG_ENV_IS_NOWHERE=y
CONFIG_ENV_IS_IN_MMC=y
CONFIG_ENV_IS_IN_SPI_FLASH=y
CONFIG_ENV_IS_IN_UBI=y
CONFIG_ENV_UBI_PART="UBI"
CONFIG_ENV_UBI_VOLUME="uboot_config"
CONFIG_ENV_UBI_VOLUME_REDUND="uboot_config_r"

I am not sure how to interpret this to find where the uboot environment is, especially since the fw_env.config file above works for all variables except bootcount. 

This topic has been closed for replies.
Best answer by ndziura

Setting CONFIG_BOOTCOUNT_ENV=y and CONFIG_BOOTCOUNT_LIMIT=y in the u-boot configuration before building fixes the problem. It also seems like upgrade_available is only used when CONFIG_BOOTCOUNT_ENV is set.

ndziura_0-1709246350585.png

 

2 replies

PatrickF
Technical Moderator
February 29, 2024

Hi @ndziura 

not expert, but from BootROM/HW perspective, there is this information

https://wiki.st.com/stm32mpu/wiki/STM32MP15_backup_registers#BOOT_COUNTER

 

from uBoot perspective

PatrickF_0-1709213596265.png

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
ndziuraAuthorBest answer
Associate
February 29, 2024

Setting CONFIG_BOOTCOUNT_ENV=y and CONFIG_BOOTCOUNT_LIMIT=y in the u-boot configuration before building fixes the problem. It also seems like upgrade_available is only used when CONFIG_BOOTCOUNT_ENV is set.

ndziura_0-1709246350585.png