STM32MP153 M4 UART core hangs after 30-60min
I have the M4 core using a UART core to send and receive data using DMA. This works just fine but over time after 30-60min the core crashes/locks up and reinitializing the UART channel does not help at all it actually crashes the sytem. Under normal operation the reinitialization sequence works properly.
The only thing I can get debug-wise is the gState which shows up as 0x21, and the state never changes after the lock-up. Reloading the m4 firmware from a7 side does not help and the UART core is broken until I do a system reboot.
Under normal operation, I do get the UART error callback triggered and the error code is 0x10, but the tx and rx continue to work without any action required.
Is there any sequence for resetting the UART physical core to recover without a reboot?
Are there any known reasons why the UART core would lock up after extended use?