Question
stm32mp157a ycoto build error :python3-setuptools-scm_2.1.0.bb:do_install
Hi,
I'm trying to build yocto environment setup for stm32mp157a Board with link https://github.com/dh-electronics/manifest-av96
during build operation i'm facing below python related error:
| + printf %b\0 bbfatal_log 'python3 setup.py install --root=/home/kaushendra/Avenger96/build-openstlinuxweston-stm32mp1-av96/tmp-glibc/work/x86_64-linux/python3-setuptools-scm-native/2.1.0-r0/image --prefix=/home/kaushendra/Avenger96/build-openstlinuxweston-stm32mp1-av96/tmp-glibc/work/x86_64-linux/python3-setuptools-scm-native/2.1.0-r0/recipe-sysroot-native/usr --install-lib=/home/kaushendra/Avenger96/build-openstlinuxweston-stm32mp1-av96/tmp-glibc/work/x86_64-linux/python3-setuptools-scm-native/2.1.0-r0/recipe-sysroot-native/usr/lib/python3.5/site-packages --install-data=/home/kaushendra/Avenger96/build-openstlinuxweston-stm32mp1-av96/tmp-glibc/work/x86_64-linux/python3-setuptools-scm-native/2.1.0-r0/recipe-sysroot-native/usr/share' execution failed.
| + exit 1
| + bb_exit_handler
| + ret=1
| + echo WARNING: exit code 1 from a shell command.
| WARNING: exit code 1 from a shell command.
| + exit 1
|
| + printf %b\0 bbfatal_log 'python3 setup.py install --root=/home/kaushendra/Avenger96/build-openstlinuxweston-stm32mp1-av96/tmp-glibc/work/x86_64-linux/python3-setuptools-scm-native/2.1.0-r0/image --prefix=/home/kaushendra/Avenger96/build-openstlinuxweston-stm32mp1-av96/tmp-glibc/work/x86_64-linux/python3-setuptools-scm-native/2.1.0-r0/recipe-sysroot-native/usr --install-lib=/home/kaushendra/Avenger96/build-openstlinuxweston-stm32mp1-av96/tmp-glibc/work/x86_64-linux/python3-setuptools-scm-native/2.1.0-r0/recipe-sysroot-native/usr/lib/python3.5/site-packages --install-data=/home/kaushendra/Avenger96/build-openstlinuxweston-stm32mp1-av96/tmp-glibc/work/x86_64-linux/python3-setuptools-scm-native/2.1.0-r0/recipe-sysroot-native/usr/share' execution failed.
| + exit 1
| + bb_exit_handler
| + ret=1
| + echo WARNING: exit code 1 from a shell command.
| WARNING: exit code 1 from a shell command.
| + exit 1
| ERROR: Function failed: do_install (log file is located at /home/kaushendra/Avenger96/build-openstlinuxweston-stm32mp1-av96/tmp-glibc/work/x86_64-linux/python3-setuptools-scm-native/2.1.0-r0/temp/log.do_install.29074)
DEBUG: Inheriting /home/kaushendra/Avenger96/layers/openembedded-core/meta/classes/python3-dir.bbclass (from /home/kaushendra/Avenger96/layers/openembedded-core/meta/classes/python3native.bbclass:1)
ERROR: Task (virtual:native:/home/kaushendra/Avenger96/layers/meta-openembedded/meta-python/recipes-devtools/python/python3-setuptools-scm_2.1.0.bb:do_install) failed with exit code '1'I searched over google but didn't find any proper solution for it
help will be appreciated.
Regards,
kaushendra