STM32MP157F-DK2 DFU mode Problem.
Hi
I have STM32MP157F-DK2 board and I am following StarterPackage Wiki document.
(https://wiki.st.com/stm32mpu/index.php/STM32MP15_Discovery_kits_-_Starter_Package)
I am following wiki and my STM32MP157F-DK2 board is not entering DFU mode.
Here are the steps I tried to enter DFU mode.
DeepSwitch is set to off and I am using 5V 3A charger for power.
I connected OTG cable and inserted microSD into slot, turned on power and pressed Reset button.
However, when I execute 'STM32_Programmer_CLI -l usb' command on PC, only 'No STM32 device in DFU mode connected' response is returned.
What did I miss?
I tested it on Windows PC and Ubuntu 20.04 PC respectively.
Any help is very appreciated, thank you,