STM32MP267FAK3 Custom Board – eMMC Flashing Timeout via STM32CubeProgrammer (No SD Card)
I am working on a custom board based on STM32MP267FAK3 and facing issues while flashing eMMC directly using STM32CubeProgrammer.
Hardware Details
SoC: STM32MP267FAK3
DDR: DDR3L (part no: MT41K512M16VRP-107 )
eMMC: Custom eMMC MX52LM08A11XVW
SD Card: Not populated / no SD card provision on board
Software Changes Done
I have already made board-specific changes in:
TF-A (DDR + PMIC configuration generated using CubeMX tool)
OP-TEE
U-Boot
Linux kernel
Flashing Method
Flashing eMMC directly using STM32CubeProgrammer
Interface: USB (DFU)
Using a TSV file generated from the build system (same method as reference BSP)
TSV File
Problem Description
When flashing the eMMC, I consistently get a timeout error in STM32CubeProgrammer.

My questions are:
1. What might be the reason for this error?
2. What are the possible solutions I can adopt to resolve this issue?
3. Is there any other way to directly flash eMMC without SD card and without using STM32CubeProgrammer?