Uboot not seeing the sd card that it was loaded from
When I start uboot it says MMC: STM32 MMC: SD/MMC:0 and STM32 SD MMC: 1 but then it won't boot linux saying "No block device". I have looked at the eval board DTS and tried to include as much relevant items as I could but am not getting any signs of life. The mmcinfo and mmc commands show nothing except the list command which just shows the same STM32 MMC: SD/MMC:0 and STM32 SD MMC: 1. I have added cd-gpios to the sdmmc1 with the gpio active low and confirmed with the gpio command that the cd pin is low when a card is present. Hoping someone can point me in the right direction.