Skip to main content
Associate
December 9, 2025
Solved

Unable to boot starter package for STM32MP257 DK - mmc device not found

  • December 9, 2025
  • 2 replies
  • 648 views

I'm currently trying to boot STM32MP257 DK board.
I managed to do it in the past with starter and developer package. I recently got back to it and tried to boot it again but without success.

I tried to upload starter package to SD card and EMMC, both ways are not working.

I followed guide on https://wiki.st.com/stm32mpu/wiki/STM32MP25_Discovery_kits_-_Starter_Package

STM32 programmer is able to see the device:

❯ STM32_Programmer_CLI -l usb
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------

===== DFU Interface =====

Total number of available STM32 device in DFU mode: 1

Device Index : USB1
USB Bus Number : 001
USB Address Number : 006
Product ID : USB download gadget@Device ID /0x505, @Revision ID /0x0011, /STM32MP257FAK Rev.Y,
Serial number : 003B002E4136500C00373653
Firmware version : 0x0110
Device ID : 0x0505

However, each time I try to upload image to the SD card I get following error:

$> STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp257f-dk-optee.tsv

Message from Embedded Flash Loader : mmc device 0 not found
Received PhaseID == 0xFF, system is going to reboot

I tried already 4 different SD cards and none of them work

I tried uploading image to EMMC and it works (flashing is complete):

STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/optee/FlashLayout_emmc_stm32mp257f-dk-optee.tsv

but then after I change boot pins to boot from EMMC (0100) there is absolutely no sign of life from the board - nothing on HDMI, nothing on serial console though ttyACMx devices are detected.

When not connected to PC, I'm using PSU for Raspberry Pi: 5.1 V, 3.1 A, 15.3W

Have I missed something? How can I make my board work or run more diagnostics?

 

Best answer by Surcouf7

Something very strange happened - all the time I had CSI camera module connected to the board. When I unplugged it, the flashing of starter package finished with success.

 

Could anybody tell me what happened and why does it work that way? 

2 replies

Surcouf7AuthorBest answer
Associate
December 9, 2025

Something very strange happened - all the time I had CSI camera module connected to the board. When I unplugged it, the flashing of starter package finished with success.

 

Could anybody tell me what happened and why does it work that way? 

PatrickF
Technical Moderator
December 10, 2025

Hi @Surcouf7 

please double check for potential supply issue.

PWR led (LD6) must be light green. Orange mean it is limited and could not be enough when activity increase (or adding external boards like CSI). Additionally LD11 is showing the supply is going to STPMIC25

USB must be Type-C 5V 3A capable with correct Power Delivery signalling (not always true on supply we could found). 

 

For Sd-Card, maybe an issue with the SD-Card holder (is it clicking well ?)

 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Associate
December 9, 2025

It looks like the board is not detecting the SD card at all, which causes the “mmc device 0 not found” error. Since different SD cards give the same result and eMMC boot also shows no output, it may be a boot pin, power, or bootloader issue. Double-check the boot switch settings, try flashing a clean starter package, use a stable USB-C power source, and check the UART output from the moment you power on. If the SD interface still does not appear, there may be a hardware problem on the board.