Unable to connect to AP using the hotstap service
Hi,
I am compiling a yocto custom layer, I am using this layers
poky/meta-poky \
poky/meta-yocto-bsp \
meta-openembedded/meta-oe \
meta-openembedded/meta-python \
meta-st-stm32mp \
custom-image \I was able to connect the LBEE5KL1DX Murata module to wifi via STA, however, I would like to use switch to the AP mode, I followed the steps in the post https://wiki.stmicroelectronics.cn/stm32mpu/wiki/How_to_configure_a_WLAN_interface_on_hotspot_mode
After that, i am able to see the AP when I look in a smartphone, but after logging with the password configured, I see the message "IP configuration failure " on my smartphone.
One thing I see suspicious is the inet when i run the command "ifconfig"

Another thing i see weird is when i run the "networkctl status wlan0" command, specifically the Network File variable

I also tried executing the bash script from a repository and it didn't work either https://github.com/STMicroelectronics/meta-st-openstlinux/blob/dunfell/recipes-samples/hotspot-wifi/files/st-hotspot-wifi-service.sh
Any help is very appreciated, thank you,
ObedPH