Skip to main content
Associate
January 26, 2026
Question

When performing heterogeneous communication with STM32MP157DAA1, the initialization function fails to enter

  • January 26, 2026
  • 1 reply
  • 223 views

Dear experts, why, under the same configuration for heterogeneous core communication, in the generated code, the debug section of the routine's initialization functions of IPPC and OPENAMP can be accessed, but the ones generated by ourselves cannot?

The following picture was generated by myself.

110330avtzk81zk2txxdkv.jpg

The following picture was generated by myself.

110406t7w9c84ypy4thyhq.jpg

Why does the routine configuration add an extra "remote" and "setting" in the file attributes?

110442g6ctgg7ztb2g6qit.jpg

But there is none in the project that was generated by myself!

110442g6ctgg7ztb2g6qit.jpg

Seeking help online, dear experts!

 

1 reply

linkAuthor
Associate
January 26, 2026

Note: The second picture is an example screenshot from the process.