Skip to main content
Associate II
September 23, 2024
Question

Access to DDR in M4

  • September 23, 2024
  • 2 replies
  • 2042 views

Deaers,

I'm using stm32mp151fad and would like to transfter sram data to ddr in M4 side. I refer to the logic analyzer example https://github.com/STMicroelectronics/logicanalyser. The sram data could be copied into ddr immediately.  

 

// mask and transfer first SRAM buff
 
        uint32_t * pSource = (uint32_t *)&mSampBuff[0];
        uint32_t * pDest = (uint32_t *)(mArrayDdrBuff[mArrayDdrBuffIndex].physAddr+mRollingCompSampCount);
        // we have a buffer of mSramPacketSize/2 bytes, to send by packet of 4 => loop on mSramPacketSize/8
        for (int i=0; i<mSramPacketSize/8; i++) {
        *(pDest+i) = *(pSource+i) & 0x7F7F7F7F; // 76µs to perform this operation, a memcpy takes 104µs
        }
 
But when I tried it, the program will go to crash. The destination address is 0xf7841000.
 
Here is my etzpc configuration in tf-a. and I use spmin instead of optee.
DECPROT(STM32MP1_ETZPC_DDRCTRL_ID, DECPROT_NS_R_S_W, DECPROT_LOCK)
DECPROT(STM32MP1_ETZPC_DDRPHYC_ID, DECPROT_NS_R_S_W, DECPROT_LOCK)

Do you have any thoughts about its root cause?

2 replies

Associate II
September 28, 2024

I use 1GB DDR. And I find it's strange that M4 could write/read DDR address 0xd0000000, but 0xf7841000 still can't. Do I misconfigure anything? The DDR size is already to set to 1GB in device tree.

Jean-Christophe_TROTIN
ST Employee
October 4, 2024

Hi @fantasylsdo,

 

About the DDR configuration, I would like to point out the following wiki article: https://wiki.st.com/stm32mpu/wiki/How_to_configure_a_256MB_DDR_mapping_from_STM32_MPU_Distribution_Package.

It might be useful to cross-check if you configure correctly for 1GB DDR.

 

Hope this information helps.

 

Regards,

JC.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
October 6, 2024

Hello Christphone,

Thanks for your kind reply. I checked the dts. The memory size is 1GB.

memory@c0000000 {
device_type = "memory";
reg = <0xC0000000 0x40000000>;
};

 

And here is the output of /proc/iomem.

c0000000-cfffffff : System RAM
c0008000-c0ffffff : Kernel code
c1100000-c125dd3f : Kernel data
d3200000-fffffffe : System RAM

Do I mis-configure other things?

 

Regards,

fantasylsdo