Skip to main content
Visitor II
May 5, 2025
Question

AI model for stm32Mp157(cortexM4)

  • May 5, 2025
  • 0 replies
  • 452 views

I am encountering an issue while analyzing my model with STM32CubeMX using X-CUBE-AI for the STM32MP1 platform. The analysis fails with the following error message:

ST Edge AI Core v2.0.0-20049
E102(CliArgumentError): stm32mp2 component is not available, please install this one

  • I am using STM32CubeMX with the X-CUBE-AI package (v10.0.0).(on windows10 PC host)

  • I am trying to analyze a model (2dcnn.h5) that I want to deploy on the STM32MP1.

  • The error indicates that the stm32mp2 component is not available and requests its installation.

My questions are:

  • What is the stm32mp2 component, and how can I install it to resolve this error?

  • Is there any additional configuration required in STM32CubeMX to support STM32MP157 when analyzing models for deployment?

  • Is there a known issue with X-CUBE-AI that might be causing this error?