Skip to main content
Associate III
January 20, 2025
Solved

AN5861 - Power rating for R4 (8R2)

  • January 20, 2025
  • 2 replies
  • 1261 views

Is there a recommended minimum SMT package size and power rating for resistor R4 (8R2) please?

Best answer by Peter BENSCH

R4 is only connected to GND by Q1 for a very short time, defined by the monoflop U1 with R3/C3, so that the heating of R4 is almost negligible depending on its dimensioning. With the approx. 0.4ms (100k, 5.6nF) from AN5861, a resistor size of 0805 is certainly sufficient.

Hope that helps?

Regards
/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
January 20, 2025

R4 is only connected to GND by Q1 for a very short time, defined by the monoflop U1 with R3/C3, so that the heating of R4 is almost negligible depending on its dimensioning. With the approx. 0.4ms (100k, 5.6nF) from AN5861, a resistor size of 0805 is certainly sufficient.

Hope that helps?

Regards
/Peter

alwAuthor
Associate III
January 20, 2025

Hi Peter,

Thanks very much.

Kind regards,

Al