Skip to main content
mikesponk2
Associate III
June 7, 2023
Solved

Black screen when enabling galcore

  • June 7, 2023
  • 4 replies
  • 6539 views

Many thanks for your help!

I have a custom STM32MP157c boards that works OK when the galcore.ko module is not deployed.

When the galcore,ko module is deployed, the screen doesn't show up the usual image and after the boot image has been displayed, it stays black.

From cat /home/weston/weston.log, it seems that something foes wrong with a signal 15 ([11:24:37.793] caught signal 15:(

[11:24:17.605] Output 'DPI-1' enabled with head(s) DPI-1
 
[11:24:17.605] Compositor capabilities:
 
 arbitrary surface rotation: yes
 
 screen capture uses y-flip: no
 
 cursor planes: yes
 
 arbitrary resolutions: no
 
 view mask clipping: yes
 
 explicit sync: no
 
 color operations: no
 
 presentation clock: CLOCK_MONOTONIC, id 1
 
 presentation clock resolution: 0.000000001 s
 
[11:24:17.606] Loading module '/usr/lib/weston/desktop-shell.so'
 
[11:24:17.609] launching '/usr/libexec/weston-keyboard'
 
[11:24:17.612] Warning: support for deprecated wl_shell interface is enabled. Please migrate legacy clients to xdg-shell.
 
[11:24:17.613] Loading module '/usr/lib/weston/systemd-notify.so'
 
[11:24:17.614] launching '/usr/libexec/weston-desktop-shell'
 
[11:24:37.793] caught signal 15
 
[11:24:37.825] output for input device event0 removed
 
[11:24:37.830] event0 - generic ft5x06 (79): device removed
 
[11:24:37.833] BUG: layer_list is not empty after shutdown. Calls to weston_layer_fini() are missing somwhere.
 
Date: 2023-06-07 UTC
 
[11:25:26.648] weston 10.0.0
 
 https://wayland.freedesktop.org
 
 Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
 
 Build: 10.0.0

From dmesg, the galcore seems loaded OK

[ 22.255642] dwc2 49000000.usb-otg: bound driver configfs-gadget
 
[ 24.262156] galcore: loading out-of-tree module taints kernel.
 
[ 24.311348] Galcore version 6.4.9.436021
 
[ 27.481105] cfg80211: Loading compiled-in X.509 certificates for regulatory database

The modinfo seems OK

root@stm32mp1:~# modinfo galcore
 
filename: /lib/modules/5.15.67/extra/galcore.ko
 
import_ns: VFS_internal_I_am_really_a_filesystem_and_am_NOT_a_driver
 
license: Dual MIT/GPL
 
description: Vivante Graphics Driver
 
alias: of:N*T*Cvivante,gcC*
 
alias: of:N*T*Cvivante,gc
 
alias: of:N*T*Cst,gcnanoC*
 
alias: of:N*T*Cst,gcnano
 
depends:
 
name: galcore
 
vermagic: 5.15.67 preempt mod_unload modversions ARMv7 p2v8
 
 
root@stm32mp1:~# uname -a
 
Linux stm32mp1 5.15.67 #12 PREEMPT Wed May 17 13:36:18 CEST 2023 armv7l armv7l armv7l GNU/Linux

The modversion of the modules seems OK:

root@stm32mp1:~# modprobe --dump-modversions /lib/modules/5.15.67/kernel/net/mac80211/mac80211.ko | grep "module_layout"
 
0x168d302d module_layout
 
root@stm32mp1:~# modprobe --dump-modversions /lib/modules/5.15.67/kernel/lib/ | grep "module_layout"
 
crc-ccitt.ko crc-itu-t.ko crc4.ko crypto/ libcrc32c.ko ts_bm.ko ts_fsm.ko ts_kmp.ko
 
root@stm32mp1:~# modprobe --dump-modversions /lib/modules/5.15.67/kernel/lib/libcrc32c.ko | grep "module_layout"
 
0x168d302d module_layout
 
root@stm32mp1:~# modprobe --dump-modversions /lib/modules/5.15.67/extra/galcore.ko | grep "module_layout"
 
0x168d302d module_layout

Is signal 15 the clue to investigate?

Can you help me debug the reason for signal 15?

Many thanks again

Michele

This topic has been closed for replies.
Best answer by mikesponk2

The error was that I was using the 6.4.6 version of the galcore driver, instead of using the 6.4.7 HAL version of the SDK that can be easily found in .../STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sources/arm-ostl-linux-gnueabi/gcnano-driver-stm32mp-6.4.7-stm32mp1-r1-rc2-r0/gcnano-driver-6.4.7

4 replies

mikesponk2
Associate III
June 7, 2023

Hi, I add this information from weston --tty=1 --debug:

root@stm32mp1:~# weston --tty=1 --debug
Date: 2023-06-07 UTC
[14:54:03.229] weston 10.0.0
 https://wayland.freedesktop.org
 Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
 Build: 10.0.0
[14:54:03.229] Command line: weston --tty=1 --debug
[14:54:03.229] OS: Linux, 5.15.67, #12 PREEMPT Wed May 17 13:36:18 CEST 2023, armv7l
[14:54:03.230] Flight recorder: enabled
[14:54:03.230] Using config file '/etc/xdg/weston/weston.ini'
WARNING: debug protocol has been enabled. This is a potential denial-of-service attack vector and information leak.
[14:54:03.231] Output repaint window is 100 ms maximum.
[14:54:03.231] Loading module '/usr/lib/libweston-10/drm-backend.so'
[14:54:03.249] initializing drm backend
[14:54:03.249] Trying logind launcher...
[14:54:03.251] logind: failed to get session seat
[14:54:03.251] logind: cannot setup systemd-logind helper error: (No data available), using legacy fallback
[14:54:03.251] Trying weston_launch launcher...
[14:54:03.251] could not get launcher fd from env
[14:54:03.251] Trying direct launcher...
[14:54:03.260] using /dev/dri/card0
[14:54:03.260] DRM: supports atomic modesetting
[14:54:03.260] DRM: supports GBM modifiers
[14:54:03.260] DRM: supports picture aspect ratio
[14:54:03.260] Loading module '/usr/lib/libweston-10/gl-renderer.so'
[14:54:03.289] EGL client extensions: EGL_EXT_client_extensions
 EGL_EXT_platform_base EGL_KHR_platform_wayland
 EGL_EXT_platform_wayland EGL_KHR_platform_gbm
[14:54:03.289] failed to initialize display
[14:54:03.290] EGL error state: EGL_NOT_INITIALIZED (0x3001)
[14:54:03.290] failed to initialize egl
[14:54:03.290] BUG: layer_list is not empty after shutdown. Calls to weston_layer_fini() are missing somwhere.
[14:54:03.290] fatal: failed to create compositor backend
Internal warning: debug scope 'drm-backend' has not been destroyed.

mikesponk2
Associate III
September 6, 2023

Hi! Anyone have any idea why the EGL fails to initialize the display? In pixman mode, all works fine.

mikesponk2
Associate III
September 6, 2023

I wonder if anybody can suggest me how to debug the EGL library for STM32MP1; anybody knows where the source files are located?

mikesponk2
Associate III
September 8, 2023

 I have enabled the galcore DEBUG mode and I see that there is a probl;em with some structures size... from dmesg:

[ 36.355766] drv_ioctl(1012): input or/and output structures are invalid:exp 376 bytes,in 424,out 0,filp=55787860 ioctlCode=0 arg=3266442176
[ 36.372427] gcmkONERROR: status=-1(gcvSTATUS_INVALID_ARGUMENT) @ drv_ioctl(1015)
[ 36.428139] drv_ioctl(1012): input or/and output structures are invalid:exp 376 bytes,in 424,out 0,filp=55787860 ioctlCode=0 arg=3268850048
[ 36.454061] gcmkONERROR: status=-1(gcvSTATUS_INVALID_ARGUMENT) @ drv_ioctl(1015)
[ 36.463382] Process 1085 has entries in its database:
[ 36.473490] gcmkONERROR: status=-1(gcvSTATUS_INVALID_ARGUMENT) @ gckOS_UnmapMemoryEx(1345)
mikesponk2
Associate III
September 8, 2023

I managed to solve the GPU problem installing the version 6.4.6 of the GPU galcore driver:

 

[ 23.608541] galcore: loading out-of-tree module taints kernel.
[ 23.777721] Init with Level=1, Zone=0x0FFFFFFF
[ 23.784846] Galcore version 6.4.6.342038
[ 23.793471] gckOS_ImportAllocators(171) Allocator: dma
[ 23.800798] gckOS_ImportAllocators(171) Allocator: user
[ 23.809218] gckOS_ImportAllocators(171) Allocator: dma
[ 23.817537] gckOS_ImportAllocators(171) Allocator: dmabuf
[ 23.827156] gckOS_ImportAllocators(171) Allocator: reserved-mem
[ 23.858760] [drm] Initialized vivante 1.0.0 20170808 for 59000000.gpu on minor 1

 But nonetheless, the egl cannot initialize the display, as I can see from the weston.log):

[15:47:43.168] logind: session control granted
[15:47:43.256] using /dev/dri/card0
[15:47:43.257] DRM: supports atomic modesetting
[15:47:43.257] DRM: supports GBM modifiers
[15:47:43.257] DRM: supports picture aspect ratio
[15:47:43.272] Loading module '/usr/lib/libweston-10/gl-renderer.so'
[15:47:43.361] EGL client extensions: EGL_EXT_client_extensions
 EGL_EXT_platform_base EGL_KHR_platform_wayland
 EGL_EXT_platform_wayland EGL_KHR_platform_gbm
[15:47:43.364] failed to initialize display
[15:47:43.364] EGL error state: EGL_NOT_INITIALIZED (0x3001)
[15:47:43.364] failed to initialize egl
[15:47:43.377] BUG: layer_list is not empty after shutdown. Calls to weston_layer_fini() are missing somwhere.
[15:47:43.377] fatal: failed to create compositor backend

 Anyone has an idea about how to debug what is happening inside the eglInitialize() function thjt fails?

mikesponk2
mikesponk2AuthorBest answer
Associate III
September 8, 2023

The error was that I was using the 6.4.6 version of the galcore driver, instead of using the 6.4.7 HAL version of the SDK that can be easily found in .../STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sources/arm-ostl-linux-gnueabi/gcnano-driver-stm32mp-6.4.7-stm32mp1-r1-rc2-r0/gcnano-driver-6.4.7