Skip to main content
Associate II
September 26, 2023
Solved

Blob transfer using BFA001V2 has an issue?

  • September 26, 2023
  • 1 reply
  • 1226 views

Hi,
I use the BFA001V2 board as a counterpart for testing IO-Link Master with BLOB transfer. A problem was detected while reading a BLOB.
When using BFA001V2, after 15 successful data transfers (flow_control set to 0x2F), an invalid flow_control with a value of 0x30 (last frame) is sent. (However, the total size of the blob must be 16 KB!).
According to the IO-Link specification, flow_control should cycle from 0x20 to 0x2F, after almost all bytes have been sent, the Last_block command (0x30) should be sent with the last block of data.
BlobSpec.png

 


Could someone check the stack on BFA001V2?
Thanks in Advance D.Krush

This topic has been closed for replies.
Best answer by Semiory

Dismis :)
Problem solved by the updating of the IO-Link Master Stack. Sorry.

1 reply

SemioryAuthorBest answer
Associate II
September 26, 2023

Dismis :)
Problem solved by the updating of the IO-Link Master Stack. Sorry.