Skip to main content
LZhan.22
Associate
October 19, 2023
Question

Bring up the STM32MP135x - Share Training Course (II)

  • October 19, 2023
  • 0 replies
  • 4391 views

This article will take MYIRMYD-YF13X and STM32MP135F-DK as examples, and continue to explain how to use STM32CubeMX combined with the developer package to implement the booting of the minimal system.
https://www.myirtech.com/news_list.asp?id=879

Following "Bring up the STM32MP135x - ST Training Course based on MYD-YF13X (I)"

4. USB Boot

USB boot is used for burning im4.1.3 PWR

Power age to external flash, e.g. NAND, SD card, etc. The burning image from PC to external flash is completed by U-Boot combined with STM32Cube Programmer. Configuring and compiling U-Boot is a precondition for burning.

According to the STM32 MPU boot sequence:
TF-A->OP-TEE->U-BOOT->Linux Kernel

Loading U-Boot into the DDR depends on TF-A and OP-TEE, sothe configuration and compilation of TF-A, OP-TEE and U-Boot need to be completed in the USB boot phase.

4.1 USB Boot: TFA Configuration and Compilation

During the USB booting stage, the TFA needs to be configured with the following peripherals: Debug serial port UART, Clock RCC, Power Supply and DDR.

4.1.1 Debugging Serial Port UART

1. Review the schematic and find the debug serial port:

stcourse201.jpg

stcourse202.png

2. Enable UART4, configure the pins and the clock:

stcourse203.png

stcourse204.png

stcourse205.png

Note: The clock for USART4 is using HSI, one reason is to refer to the clock tree configuration of STM32MP135F-DK, and the other reason is to consider the application of serial port wake-up in low-power working mode. Excluding these two points, other clock sources can also be used.

3. Click "Generate code", and add the user code for the serial port configuration of the TFA stage.

Open the generated STM32CubeMX project, open the TF-A device tree (stm32mp135d-myir_bring_up-mx.dts), and add the nodes "choosen" and "aliases" at the "USER CODE BEGIN root".

/* USER CODE BEGIN root */

aliases {

serial0 = &uart4;

};

chosen {

stdout-path = "serial0:115200n8";

};

/* USER CODE END root */

4. (Optional) Compile the TFA USB image and deploy to the board.

Compile:

PC $> cd

PC $> source

PC $> make -f ../Makefile.sdk TF_A_CONFIG=usb TF_A_DEVICETREE=stm32mp135d-myir_bring_up-mx stm32

Deploy (please make sure the board is powered up, the serial cable and the USB cable are correctly connected before deploying):
PC $> STM32_Programmer_CLI -c port=usb1 -d ../deploy/tf-a-stm32mp135d-myir_bring_up-mx-usb.stm32 0x1 -s 0x1

Serial port printing:

NOTICE:  CPU: STM32MP135F Rev.?

NOTICE:  Model: STMicroelectronics custom STM32CubeMX board - openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23

ERROR:   nvmem node board_id not found

WARNING: VDD unknown

INFO:    Reset reason (0x35):

INFO:      Power-on Reset (rst_por)

INFO:    FCONF: Reading TB_FW firmware configuration file from: 0x2ffe0000

INFO:    FCONF: Reading firmware configuration information for: stm32mp_io

INFO:    Using USB

INFO:      Instance 2

INFO:    Boot used partition fsbl1

NOTICE:  BL2: v2.6-stm32mp1-r2.0(debug):v2.6-stm32mp-r2-4-g2dedc1cf0-dirty(2dedc1cf)

NOTICE:  BL2: Built : 02:45:42, Jun  6 2023

INFO:    BL2: Doing platform setup

ERROR:   Invalid DDR init: error -22

PANIC at PC : 0x2ffe7739

Exception mode=0x00000016 at: 0x2ffe7739

5. Troubleshooting

If the serial port prints as follows in the previous step or does not print anything:

PANIC at PC : 0x2ffe7739

Exception mode=0x00000016 at: 0x2ffe7739

Then please confirm:

  • Whether the User code has been added to the correct location.
  • Whether the Debug serial port is UART4 and make sure the PIN is configured correctly.
  • Check the hardware connection.

4.1.2 DDR

The following points need to be noted for the DDR configuration:

  • SDRAMS size
  • One/two pieces (16/32 bits), STM32MP13x DDR is 16bits, so the configurations are all using 1 piece of SDRAM.
  • DDR types: DDR3/DDR3L/LPDDRx
  • DDR frequency

1. Check the schematic diagram of the DDR design section, confirm the size and frequency and other parameters, and complete the design of the DDR part.

Below are some examples of different DDR designs and their corresponding configurations:

Example 1: STM32MP157C-EV1, two pieces of SDRAM, 32bits, 1GBytes

stcourse206.jpg

stcourse207.jpg

stcourse208.png

stcourse209.png

The DDR frequency can be configured in the Configuration interface.

Example 2: STM32MP135F-DK, one piece of SDRAM, 16bits, 512Mbytes.

stcourse210.png
stcourse211.png

stcourse212.png

stcourse209.png

Now lets take a look at the DDR design part of MYIRs MYD-YF13X board:

stcourse214.pngstcourse215.png

One piece of SDRAM, 16bits, 256Mbytes, STM32CubeMX configured as follows:

stcourse216.png

stcourse217.png

 

 

This topic has been closed for replies.