Skip to main content
Associate II
June 19, 2023
Question

Can I use pyinstaller on Ubuntu to bundle Python code into an executable file and run it on STM32?

  • June 19, 2023
  • 1 reply
  • 5122 views

 

Hello,

I am a newcomer to embedded systems. I have a STM32MP157D-DK1 and I'm planning to develop some python applications to run on the A7 processor. I am encountering some issues.

1. I created a simple web application using Python on Ubuntu. (python module: Flask)
2. I confirmed that it can be executed successfully.
3. I bundled it into a single executable file using pyinstaller (PC $> pyinstaller app.py --onefile).
4. I verified that the executable file can be used properly.
5. I transferred the file to an STM32 (starter kit).
6. When I tried to execute the file, an error occurred.
Error Message:
./app: line 1: syntax error: unexpected ")"

Other experiments:
I try to execute python source code directly on STM32, there is no problem.
I try to bundle python code into a single executable on STM32, but can't install pyinstaller. (pip3 install pyinstaller)

Thanks for your support,
Ken.

1 reply

Jean-Marc B
ST Employee
June 26, 2023

Hi @Ken_102633 

The app you created with pyinstaller from your PC running ubuntu is compiled for an architecture compatible with your PC (most probably x86_64). However, STM32MP15 boards rely on a ARM architecture hence can't run x86_64 app. That explains the error you got in your 6th step.

Then, installing pyinstaller from pip3 shows errors as some build dependencies are not available such as a gcc toolchain. To bypass these dependencies, you need to build your own distribution and setup your own repository (please refer to https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution#How_to_activate_a_local_package_repository )

Once your repository is activated, install the package group core-buildessential:

 

root@stm32mp1:~# apt-get update
root@stm32mp1:~# apt-get install packagegroup-core-buildessential
# EDITED SECTION BELOW
root@stm32mp1:~# apt-get install ldd

 

 You can now install pyinstaller with the following command:

 

root@stm32mp1:~# env PYI_STATIC_ZLIB=1 pip3 install pyinstaller

 

Then try to build your app.

Best regards,

--JM

Explorer
January 2, 2024

Thank you so much @Jean-Marc B , the steps listed here helped to install and work with pyinstaller on stm device!