Skip to main content
Visitor II
October 8, 2023
Question

Can not Flash STM32MP157FAD.The MPU restarts again and again.

  • October 8, 2023
  • 1 reply
  • 865 views

Can not Flash STM32MP157FAD. with CubeProgrammer, and StarterPackage Image. First 2 files download ok, then get "Reconnecting the device...", and it never reconnects. And the MPU reset, with CubeProgrammer can download first 1 file. Windows11cubeProgram.jpgterminal.jpg drops the USB-DFU device. How to fix?

This topic has been closed for replies.

1 reply

PatrickF
Technical Moderator
October 9, 2023

HI @xingya 

Could you please confirm you are using STM32MP157F-EV1 board or a custom board?
If you are using STM32MP157F-EV1 board, do the flashload works with provided Starter package ?

Reset reason shows IWDG2 watchdog reset, maybe something to look at.

Btw, your are using an old Ecosystem v2, which is not supported anymore. If you are still in development phase, we strongly encourage to switch to latest Ecosystem v5.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here