Skip to main content
jgauthier
Senior
May 15, 2023
Solved

Configuring and reading "GPIO Analog"

  • May 15, 2023
  • 3 replies
  • 8028 views

Using the STM32MP157 development kit, I have configured two "GPIO Analog" lines that are exposed through CN13 (pins 1 and 2).

I am trying to set these up as such. From going down the rabbit trail of documentation:

https://wiki.st.com/stm32mpu/wiki/GPIO_internal_peripheral#Software_frameworks

https://wiki.stmicroelectronics.cn/stm32mpu/wiki/GPIOLib_overview

and then:

https://wiki.stmicroelectronics.cn/stm32mpu/wiki/Overview_of_GPIO_pins

https://wiki.stmicroelectronics.cn/stm32mpu/wiki/Pinctrl_overview

It seems to confirm that I need to use "pinctrl" technique to set these. Okay. I have configured them with CubeMX. However, my DTS file doesn't reference these pins at all.


_legacyfs_online_stmicro_images_0693W00000bk7OZQAY.png 

I've gone through the exported DTS and I do not see anything referencing PG3, or PH6.

So, I feel like this has failed at the outset.

Is there a trick to this? I assume once I get these configured I can read the value using libgpio API functions.

This topic has been closed for replies.
Best answer by PatrickF

I agree ADC connections are quite complex to fully master.

Best for this ADC pin choice is to use CubeMX.

You could find information in Product Reference Manual, ADC section

e.g.


_legacyfs_online_stmicro_images_0693W00000bkCAIQA2.pngtogether with Product Datasheet pin list, looking in additional function column


_legacyfs_online_stmicro_images_0693W00000bkCAXQA2.pngRegards.

3 replies

PatrickF
Technical Moderator
May 16, 2023

Hi @Community member​ 

I think CubeMX does not generate anything in pinctrl unless those pins are used by a peripheral.

If you want to keep GPIO in analog mode to save power (barely visible gain), you don't have to do anything as this is the default setting.

Does analog mean you are asking for ADC conversion ?

If yes, please had a look to

https://wiki.st.com/stm32mpu/wiki/ADC_device_tree_configuration

https://wiki.st.com/stm32mpu/wiki/ADC_OpenSTLinux_drivers

https://wiki.st.com/stm32mpu/wiki/IIO_overview

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
jgauthier
jgauthierAuthor
Senior
May 16, 2023

Thank you for your answer. I want the GPIO in analog mode to read input from it. I have looked at all those pages. I am currently using the ADC channels for a few inputs. Following those readings I did not attempt to apply those to GPIO Analog inputs. I can. To this section, I could add:

adc_pins_mx: adc_mx-0 {
 pinmux = <STM32_PINMUX('G', 3, ANALOG)>; /* GPIO Analog */
 <STM32_PINMUX('H', 6, ANALOG)>; /* GPIO Analog */
 }

(There are other items in this list, I just abbreviated it)

Then, if I go a bit down I've previously added input channels like so

	adc1:adc@0{
		status = "okay";
 
		channel@0{
			reg = <0>;
			st,min-sample-time-ns = <5000>;
		};
 
	};

But these all reference "channel" which is the INP number on the ADC channel. The GPIO does not have an ADC channel ... I don't know how to expose it. The documentation makes sense - but not for the GPIO analog inputs. So I am looking to close that configuration/knowledge gap.

PatrickF
Technical Moderator
May 16, 2023

Hi,

Please refer to product datasheet pinout to see which GPIO have ADC capabilities.

All GPIOs have analog mode (for power saving in order to disable logic driver and receiver), but this does not mean there is an ADC connected to it.

There is no way to 'read' from GPIO analog unless using ADC to acquire the analog voltage on available ADC channels on specific GPIO pins.

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
jgauthier
jgauthierAuthor
Senior
May 16, 2023

Thank you. That actually makes perfect sense. They are all analog capable, as it's just a setting to lower power. However, to read actual analog signal they must be attached to an internal ADC peripheral. The datasheet is sparse. However, the Reference Manual has quite a bit of information about GPIOs. What I don't see is an indication about what GPIO inputs might have an ADC backend. But I'm not sure what exactly I am looking for in that regard.

PatrickF
PatrickFBest answer
Technical Moderator
May 16, 2023

I agree ADC connections are quite complex to fully master.

Best for this ADC pin choice is to use CubeMX.

You could find information in Product Reference Manual, ADC section

e.g.


_legacyfs_online_stmicro_images_0693W00000bkCAIQA2.pngtogether with Product Datasheet pin list, looking in additional function column


_legacyfs_online_stmicro_images_0693W00000bkCAXQA2.pngRegards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here