Skip to main content
Associate II
July 10, 2025
Question

DDR Contention

  • July 10, 2025
  • 1 reply
  • 265 views

Hello,

I am running on a stm32mp255dak processor with Linux running on the A35 core and FreeRTOS on the M33 core. I am running the M33 core code out of DDR.

I am seeing an issue where the M33 core performance takes a hit and missed deadlines when the A35 core loads the DDR. The issue is very similar to the one described in this forum. 

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1220944/am625-lpddr4-access-priority

 

Does anyone know where to start looking to find the root cause of this issue? I done some investigation into the DDRCTRL registers and tired to mess if the QoS of the A35 core, but that did not seem to make a difference. It seems like the issue is a DDR contention issue between the two cores.

1 reply

PatrickF
Technical Moderator
July 11, 2025

Hi @nielsenni101 

I cannot help you for DDR prioritization or else settings .

Maybe a dumb question, is ICACHE and DCACHE enabled on M33 for DDR accesses (I hope so) ?

When your have some hard real time, it would be necessary to have some portion of the code or critical data inside  SRAMs.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Associate II
July 11, 2025

Hi @PatrickF ,

 

Yes ICACHE and DCACHE is enabled on the M33 core. I have been experimenting with putting some of the critical code into SRAM. So far I have not seen any improvement from that, but I am still in the process of getting more into SRAM (unfortunately the binary is way to big to fit into SRAM). I would expect ICACHE and DCACHE to help here but maybe I am getting a lot of cache misses so it is not really helping? Is there a way to tell if ICACHE and DCACHE are actually helping?

This issue seems to be common to other heterogeneous processor architectures (see the link I made in the OP). So I was hoping that there was a known solution to this issue other then just using SRAM because of the large binary size.