Skip to main content
Associate
April 2, 2024
Question

EFI boot based on openstlinux-6.1 for stm32mp using emmc storage

  • April 2, 2024
  • 1 reply
  • 1611 views

Good morning, I've been trying to get EFI boot working from emmc. After configuring flash layouts to contain fat32 efi partition and getting through uboot and optee configuration to properly flash using cube programmer, I can't seem to figure out why the uboot fails to load the EFIed kernel during boot process. Screenshot from 2024-04-02 13-54-29.pngIt would seem as if the kernel image is missing the efi stub, but my kernel config would suggest otherwise.

Davidomil_0-1712091604574.png

Any ideas on how to get the EFI boot to work? 

This topic has been closed for replies.

1 reply

Erwan SZYMANSKI
Technical Moderator
April 5, 2024

Hello @Davidomil,
Did you prepare your software using Distribution package (Yocto) or Developer package (Cross compile + SDK)
Do you confirm you are aware about the different steps mentioned in this article, specially the fragment for U-Boot and the kernel ? https://wiki.st.com/stm32mpu/wiki/How_to_configure_UEFI_boot_with_the_Distribution_Package

Kind regards,
Erwan. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
DavidomilAuthor
Associate
April 18, 2024

Hello @Erwan SZYMANSKI , 

I am building from yocto environment. And my uboot efi config looks like this:

# Basic EFI configuration
# Compliant with SystemReady 1.1
#
CONFIG_BOOTM_EFI=y
CONFIG_CMD_BOOTEFI=y
CONFIG_CMD_NVEDIT_EFI=y
CONFIG_CMD_EFIDEBUG=y
CONFIG_CMD_BOOTEFI_HELLO=y
CONFIG_CMD_BOOTEFI_HELLO_COMPILE=y
CONFIG_CMD_BOOTEFI_SELFTEST=y
CONFIG_CMD_GPT=y
CONFIG_EFI_PARTITION=y
CONFIG_EFI_LOADER=y
CONFIG_EFI_DEVICE_PATH_TO_TEXT=y
CONFIG_EFI_UNICODE_COLLATION_PROTOCOL2=y
CONFIG_EFI_UNICODE_CAPITALIZATION=y
CONFIG_EFI_HAVE_RUNTIME_RESET=y
CONFIG_EFI_VARIABLE_FILE_STORE=y
# RTC: GET TIME
CONFIG_DM_RTC=y
CONFIG_EFI_GET_TIME=y
CONFIG_EFI_SET_TIME=y
CONFIG_RTC_EMULATION=y
# Capsule update
CONFIG_CMD_DFU=y
CONFIG_FLASH_CFI_MTD=y
CONFIG_EFI_CAPSULE_FIRMWARE_FIT=y
CONFIG_EFI_CAPSULE_FIRMWARE_MANAGEMENT=y
CONFIG_EFI_CAPSULE_FIRMWARE=y
CONFIG_EFI_CAPSULE_FIRMWARE_RAW=y
CONFIG_EFI_CAPSULE_FMP_HEADER=y
CONFIG_DFU_OVER_TFTP=y
CONFIG_DFU_OVER_USB=y
CONFIG_DFU_MMC=y
CONFIG_DFU_MTD=y
CONFIG_DFU_NAND=y
CONFIG_DFU_SF=y
# filesystem
CONFIG_CMD_GPT=y
CONFIG_FAT_WRITE=y
CONFIG_FS_FAT=y
CONFIG_CMD_PART=y
CONFIG_PARTITIONS=y
CONFIG_DOS_PARTITION=y
CONFIG_ISO_PARTITION=y
CONFIG_EFI_PARTITION=y
CONFIG_PARTITION_UUIDS=y
# EFI addons configuration
# If you need to load an INITRD without efi bootmgr
CONFIG_EFI_LOAD_FILE2_INITRD=y
CONFIG_EFI_INITRD_FILESPEC="mmc 0:8 st-image-resize-initrd"
CONFIG_FIT_SIGNATURE=y
CONFIG_LEGACY_IMAGE_FORMAT=y
CONFIG_EFI_SECURE_BOOT=y
# Device Firmware Upgrade
CONFIG_FIT=y
CONFIG_OF_LIBFDT=y
CONFIG_DFU=y
CONFIG_CMD_DFU=y
CONFIG_DFU_MMC=y
CONFIG_DFU_MTD=y
CONFIG_DFU_NAND=y
CONFIG_DFU_SF=y
CONFIG_DFU_OVER_TFTP=y
CONFIG_DFU_OVER_USB=y

and my kernel config 

CONFIG_EFI=y
CONFIG_EFI_STUB=y
CONFIG_EFI_VARS=y
CONFIG_EFI_VARS_PSTORE=m
CONFIG_EFI_CAPSULE_LOADER=m

# --------------------------
# Systemd
# --------------------------
CONFIG_EFIVAR_FS=y
CONFIG_EFI_PARTITION=y


# efi
CONFIG_EFI=y
CONFIG_EFI_STUB=y
CONFIG_EFI_VARS=y
CONFIG_EFI_VARS_PSTORE=y
CONFIG_EFI_CAPSULE_LOADER=y

CONFIG_EFI_GENERIC_STUB_INITRD_CMDLINE_LOADER=y
CONFIG_EFI_BOOTLOADER_CONTROL=y
CONFIG_EFI_CAPSULE_LOADER=y

# needed for lttng-modules
CONFIG_KPROBES=y
CONFIG_KALLSYMS_ALL=y

CONFIG_TEE=y
CONFIG_OPTEE=y

CONFIG_RELOCATABLE=y
CONFIG_EFI=y
CONFIG_EFI_STUB=y
CONFIG_X86_SYSFB=y
CONFIG_FB_SIMPLE=y
CONFIG_FRAMEBUFFER_CONSOLE=y

CONFIG_EFIVAR_FS=y
CONFIG_EFI_PARTITION=y
CONFIG_EFI_MIXED=y

I do have MACHINE_FEATURES += "efi" in my machine configuration