Skip to main content
GMate
Associate
August 29, 2019
Solved

Error: failed to download Segment[0]

  • August 29, 2019
  • 3 replies
  • 2775 views

Hallo,

Im trying to flash an image (st-example-image-qt-openstlinux-eglfs-stm32mp1), bu it fails on partition 0x23

this is the output on Terminal:

giomate@giolaptop:~/Development/STM32/MP15/Distribution/openstlinux/build-openstlinuxeglfs-stm32mp1/tmp-glibc/deploy/images/stm32mp2/stm32mp1$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-example-image-qt/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv -log

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.1.0          

   -------------------------------------------------------------------

Log output file:  /home/giomate/.STM32CubeProgrammer/trace.log

USB speed  : High Speed (480MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000

SN     : 0030002C3338510939303435

FW version : 0x0110

Device ID  : 0x0500

Device name : STM32MPxxx

Device type : MPU

Device CPU : Cortex-A7

Start Embedded Flashing service

Memory Programming ...

Opening and parsing file: st-example-image-qt-openstlinux-eglfs-stm32mp1.ext4

 File     : st-example-image-qt-openstlinux-eglfs-stm32mp1.ext4

 Size     : 1086306 KBytes

 Partition ID : 0x23 

Download in Progress:

[===================================        ] 70% 

Error: failed to download Segment[0]

Error: failed to download the File

Time elapsed during download operation: 00:14:00.737

Error: Download partition 0x23 failed

Error: TSV flashing service failed

I appeciate any comment or suggestions

Best answer by GMate

Yeap, it was the sizes of the roofs partition

3 replies

PatrickF
Technical Moderator
August 30, 2019

Probably linked to that issue (assigned size/offset in Flashlayout too small for your image) https://community.st.com/s/question/0D50X0000B7Ykl5SQC/getting-failure-while-compiling-qtwebkit-for-yocto

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
GMate
GMateAuthorBest answer
Associate
August 31, 2019

Yeap, it was the sizes of the roofs partition

Visitor II
March 27, 2025

 

STMicroelectronics ST-LINK GDB server. Version 7.8.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.17.0

-------------------------------------------------------------------

 

 

 

Log output file: C:\Users\rlv\AppData\Local\Temp\STM32CubeProgrammer_a26804.log

ST-LINK SN : "

ST-LINK FW : V2J45S7

Board : --

Voltage : 3.30V

SWD freq : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x461

Revision ID : Rev 2.0

Device name : STM32L496xx/STM32L4A6xx

Flash size : 512 KBytes

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0x93

Debug in Low Power mode enabled

 

 

 

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a26804.srec

File : ST-LINK_GDB_server_a26804.srec

Size : 299.71 KB

Address : 0x08000000

 

 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 277]

Download in Progress:

 

 

Error: failed to download Segment[0]

Error: failed to download the File

Encountered Error when opening C:\ST\STM32CubeIDE_1.14.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.400.202404281720\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Shutting down...

Exit.

 

Step 1: Full chip erase

Ruben_2025_0-1743054247727.png
 
Step 2: Starting Programming
Ruben_2025_1-1743054378930.png