“Error: failed to download Segment[0]�? Populate the target and boot the image example
“Error: failed to download Segment[0]�?
I looked at the other items with the same title but did not see an answer that would help me.
I am using the STM32MP157F-DK2
The demo code was working when box was opened
I tried to run the demo
“Populate the target and boot the image�?
at
https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2
I am using ecosystem release v3.1.0
And
STM32CubeProgrammer 2.9.0
Down load eventually fails with “Error: failed to download Segment[0]�?
Any help on the matter would be appreciated
Below is the Log
10:53:37 : USB speed : High Speed (480MBit/s)
10:53:37 : Manuf. ID : STMicroelectronics
10:53:37 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
10:53:37 : SN : 002A001B3438511436383238
10:53:37 : FW version : 0x0110
10:53:37 : Board : --
10:53:37 : Device ID : 0x0500
10:53:48 : Start Embedded Flashing service
10:53:48 : Memory Programming ...
10:53:48 : Opening and parsing file: tf-a-stm32mp157f-dk2-usb.stm32
10:53:48 : File : tf-a-stm32mp157f-dk2-usb.stm32
10:53:48 : Size : 225596 Bytes
10:53:48 : Partition ID : 0x01
10:53:48 : Download in Progress:
10:53:48 : File download complete
10:53:48 : Time elapsed during download operation: 00:00:00.473
10:53:48 : RUNNING Program ...
10:53:48 : PartID: :0x01
10:53:48 : Start operation done successfully at partition 0x01
10:53:48 : Flashlayout Programming ...
10:53:48 : Running Flashlayout Partition ...
10:53:48 : Flashlayout partition started successfully
10:53:48 : Memory Programming ...
10:53:48 : Opening and parsing file: fip-stm32mp157f-dk2-trusted.bin
10:53:48 : File : fip-stm32mp157f-dk2-trusted.bin
10:53:48 : Size : 1090807 Bytes
10:53:48 : Partition ID : 0x03
10:53:48 : Download in Progress:
10:53:50 : File download complete
10:53:50 : Time elapsed during download operation: 00:00:01.428
10:53:50 : RUNNING Program ...
10:53:50 : PartID: :0x03
10:53:50 : Reconnecting the device ...
10:53:53 : USB speed : High Speed (480MBit/s)
10:53:53 : Manuf. ID : STMicroelectronics
10:53:53 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
10:53:53 : SN : 002A001B3438511436383238
10:53:53 : FW version : 0x0110
10:53:53 : Board : --
10:53:53 : Device ID : 0x0500
10:53:53 : Device name : STM32MP157FAC Rev.Z
10:53:53 : Device type :
10:53:53 : Device CPU :
10:53:53 : Start operation done successfully at partition 0x03
10:53:53 : Memory Programming ...
10:53:53 : Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
10:53:53 : File : tf-a-stm32mp157f-dk2-sdcard.stm32
10:53:53 : Size : 225489 Bytes
10:53:53 : Partition ID : 0x04
10:53:53 : Download in Progress:
10:53:56 : Error: failed to download Segment[0]
10:53:56 : Error: failed to download the File
10:53:56 : Error: Download partition 0x04 failed
10:53:56 : Error: TSV flashing service failed
10:53:56 : Warning: Connection to device 0x500 is lost
10:53:56 : Disconnected from device.