Skip to main content
Senior
December 30, 2023
Solved

Failed to get controller clock i2c

  • December 30, 2023
  • 3 replies
  • 5493 views

Got this error in boot log.

[ 4.036653] stm32f7-i2c 5c009000.i2c: error -ENOENT: Failed to get controller clock
[ 4.054809] stm32f7-i2c: probe of 5c009000.i2c failed with error -2

5c009000 refers to i2c6. Below is the relevant section in the optee dts. I2C4 and I2C6 share a clock and I2C4 is working fine. I2C6 is mentioned in the eztpc node, so that ain't it either.

	st,clksrc=<
		CLK_CKPER_DISABLED
		CLK_ETH_PLL4P
		CLK_SDMMC12_PLL3R
		CLK_STGEN_HSI
		CLK_I2C46_HSI
		CLK_SDMMC3_PLL3R
		CLK_USBO_USBPHY
		CLK_UART24_HSI
		CLK_RNG1_CSI
		CLK_MPU_PLL1P
		CLK_AXI_PLL2P
		CLK_MCU_PLL3P
		CLK_RTC_LSI
		CLK_MCO1_DISABLED
		CLK_MCO2_DISABLED
	>;

 The i2c6 section:

&i2c6{
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&i2c6_pins_z_mx>;
	pinctrl-1 = <&i2c6_sleep_pins_z_mx>;
	status = "okay";

	pcf85263: pcf85263@51 {
		compatible = "nxp,pcf85263";
		reg = <0x51>;
		status = "okay";
	};
};

 I2C4 was set up to 400kHz and I2C6 default, changing I2C4 to default didn't help.

Am I forgetting something? Full dts can be found here.

Best answer by Erwan SZYMANSKI

Hello @michiel.tjampens ,
I think you have to do the same as for i2c4, in your core/code/dts/kernel/stm32mp151a-tios-scmi.dtsi, as to know : 

&i2c6 {
	clocks = <&scmi_clk CK_SCMI_I2C6>;
	resets = <&scmi_reset RST_SCMI_I2C6>;
};

Kind regards,
Erwan.

3 replies

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
Technical Moderator
January 2, 2024

Hello @michiel.tjampens ,
I think you have to do the same as for i2c4, in your core/code/dts/kernel/stm32mp151a-tios-scmi.dtsi, as to know : 

&i2c6 {
	clocks = <&scmi_clk CK_SCMI_I2C6>;
	resets = <&scmi_reset RST_SCMI_I2C6>;
};

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Senior
January 2, 2024

Hello @Erwan SZYMANSKI 

That did the trick.But any idea why i2c4 and i2c6 need to be mentioned in the scmi but i2c5 doesn't?

Also i2cdetect takes atleast a second per address... but does in the end find the rtc on the correct address.

Pull-ups are present, idle state is high etc.

debugging
Lead
August 5, 2024

I just fixed this same error after debugging  this for a day by adding this line in the SCMI files. This is not mentioned in the WIKI , nor CubeMX generates the SCMI file, nor the WIKI mentions about adding the clocks to OPTEE and EZTPC.

 

I now have the same issue with i2cprobe -y 0 on I2C6, is is very slow and takes one second per address. There are no devices on the bus. . I used the same code for i2cprobe for an MCU and that does not show such behavior

Is this normal or indicate a problem ? AFAIK, I2Cprobe just pulls the lines high and low and see if something happens, like basic GPIO.