Getting started with STM32MP257F-DK OpenSTLinux Starter kit and B-CAMS-IMX
Hello! I'm just getting started with an STM32MP257F-DK and B-CAMS-IMX module. I've followed the instructions for connecting the B-CAMS-IMX and have populated SD cards for booting with both optee and extensible layouts, but I am having an issue getting the camera module up and going.
Instructions in the Wiki made it seem like this module is supported out of the box, but I am getting "imx335 0-001a: failed to find sensor: -6" at boot with both SD card images. Looking at the stm32mp257f-dk dts, it seems that the other components of the B-CAMS-IMX (ToF and IMU) are not defined as well.
Am I missing something? Do I need to create a custom dts to bring up this module? Thanks for any help.