Skip to main content
Associate II
September 16, 2025
Question

how to use DDR3L with STM32mp257Fak3

  • September 16, 2025
  • 3 replies
  • 433 views

Hello 
I am planning to use STM32mp257Fak3 with DDR3L (16bit and 32 bit saperately),
can you suggest some DDR part no and it's sonnection.

3 replies

Pwxn
ST Employee
September 17, 2025

Hello @abhineetranjan 

You can refer to this 2 application notes:

https://www.st.com/resource/en/application_note/an5723-guidelines-for-ddr-configuration-on-stm32mp2-mpus-stmicroelectronics.pdf

https://www.st.com/resource/en/application_note/an5724-guidelines-for-ddr-memory-routing-on-stm32mp2-mpus-stmicroelectronics.pdf

ST follow the JEDEC standards so you should be able to choose any part that are following the same.

 

"DDR3L with a data rate of 2133 MT/s, voltage at 1.35 V. More information on DDR3L SDRAM can be found
on the JEDEC DDR3 SDRAM Standard JESD79-3F." - AN5724 2 Design interface constraints

 

I hope this will help you.

 

Regards,

Associate II
September 30, 2025

Thank you for your response,
can I use 2 , 8bit DDR3L with STM32MP257FAL3 (as this is not mentioned in the pdf you provided), to achieve 1GByte Memory density.

Best Regards
Abhineet Ranjan

Associate II
October 1, 2025

abhineetranjan_0-1759295168086.png

Block Diagram for reference....

Associate II
November 7, 2025

Hello,
I am using 16 bit DDR3L (MT41K512M16VRP-107) with STM32mp257FAK3, 
the available Nets in processor is 32 (32-bit), what should be done with the remaining Databus (should it be terminated or left floating or pull down.

Best regards,
Abhineet Ranjan

PatrickF
Technical Moderator
November 7, 2025

@abhineetranjan wrote:

Hello,
I am using 16 bit DDR3L (MT41K512M16VRP-107) with STM32mp257FAK3, 
the available Nets in processor is 32 (32-bit), what should be done with the remaining Databus (should it be terminated or left floating or pull down.

Best regards,
Abhineet Ranjan


 

Leave them open. Note that you should connect you 16-bit memory on DQ0-15.


AN5489 could help (even if DDR3 is not listed in it).
You could also have a look to provided DDR3L routing example in  (altough does not cover 16-bit DDR on 32-bit interface).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Associate II
January 27, 2026

Hello @PatrickF 
Thank you for your response

In the DDR guideline, it is mentioned
DQ or DQM to DQS_N/DQS_P +/- 56 mils (1.42 mm)
and 
DQS_N/DQS_P to CLK_N/ CLK_P +/- 475 mils (12.06 mm)

Does these mils include Pin delay (time it takes for a signal to travel from the internal silicon die to the physical package ball/pin (or vice-versa)) for length matching also. If No then can you provide the same.

Best Regards
Abhineet Ranjan

PatrickF
Technical Moderator
January 27, 2026

Hi @abhineetranjan 

Yes, those values should includes the package internal length. 
Please look into  where you could find for each package and memory choices, an excel sheet taking into account package internal length.(xxxx_Memory_length_equalization_in_mm_for_STM32MP25xxxx (xxxxx)_Template.xlsx.).

 

For you project, you could also take the ready made provided routing example layout which follows the length rules.

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Associate II
February 3, 2026

Hello Patrick,
Thank you for your help
Can we get pin delay for whole STM chip.

Best Regards
Abhineet Ranjan