HSP051-4M10 on STM32MP257-DK board?
Hi,
just a quick question to understand the hardware of the STM32MP257 development kit board: there are several ESD-protection components of type HSP051-4M10 used.
What is the exact purpose of them, are they there
a) because the DK-board is intended to be touched by users and therefore there is some higher danger these users kill that board with some electrostatic discharge when touching it
b) because this type of device is recommended to be used in general due to some components being unusual sensitive against ESD (for an example, at the RasPi I think no such protection is used)
c) something else?
Thanks for sheding some light on this :)