Skip to main content
Associate
November 22, 2024
Question

I can't set up Ethernet for the yocto project on the stm32mp257f-evboard.

  • November 22, 2024
  • 2 replies
  • 861 views

I installed the distribution package using the stm32mp257f-ev board, but eth1 is visible but eth2 is missing. How do I activate both end0 and end1 in yocto.

2 replies

hadolAuthor
Associate
November 25, 2024

I can't see the network drive even if I run it according to the address below.

https://wiki.st.com/stm32mpu/wiki/X-LINUX-TSNSWCH_Expansion_Package

hadolAuthor
Associate
November 25, 2024
watch -n1 deptp_tool --get-current-dataset


Every 1.0s: deptp_tool --get-current-dataset stm32mp2: Mon Nov 25 05:35:26 2024

ERROR: ptp_management_local.c:154 ptp_management_connect_local: Failed to connec
t to '/var/run/deptp'
ERROR: io.c:469 ptp_management_tool_connect: Failed to initialize transport