Skip to main content
Associate II
May 29, 2024
Question

Inquiry about PMIC Example in Baremetal for STM32MP13 Series?

  • May 29, 2024
  • 1 reply
  • 931 views

Hello,

I would like to set up the PMIC for the MP13 series using Baremetal. The provided PMIC-related documentation appears to be related to Linux. Is there any documentation or example available for using it with Baremetal?

Thank you.

1 reply

PatrickF
Technical Moderator
May 29, 2024

Hi @SL1 

Do the BSP provided with STM32CubeMP13 package not enough ?

https://wiki.st.com/stm32mpu/wiki/STM32CubeMP13_Package#BSP_drivers

You also have a bunch of examples running on STM32MP135F-DK which embed an STPMIC1.

https://wiki.st.com/stm32mpu/wiki/STM32CubeMP13_Package#Examples,_applications_and_demonstrations_for_STM32MP135x-DK_Discovery_kit 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
SL1Author
Associate II
June 7, 2024

Hello, sorry for the late response.

The example source is excellent, and I have also added the DISCO BSP source to my project.

However, the page below only contains information related to Linux. When creating a new project with STM32CubeMX, I don't see any settings or PACK related to the PMIC. Hence, I am writing to inquire about this.

 

https://wiki.st.com/stm32mpu/wiki/PMIC_hardware_components

 

I will conclude by adding the DISCO BSP source to the project.

 

Thank you for your response.