Skip to main content
Associate
May 31, 2024
Solved

Is it possible to make this system using stm32mp157??

  • May 31, 2024
  • 1 reply
  • 1183 views

Hello,

I would like to make the system below using stm32mp157.

- System Description -

1. 100Mbps Full-Duplex Ethernet

2. Cortex-A7 receives and transmits data from Ethernet on the PC. 

3. Cortex-A7 calculates Ethernet data and sends the result to Cortex-M4.

4. Cortex-M4 controls peripheral(SPI, I2C, UART, GPIO) using DMA and interrupt 

 

Can I implement a program like the above??

I've usually used F4 series or L4 series, so I don't know about MPU lines.

If the program is implementable, please let me know what I need to know.

If the program cannot be implemented, please recommend MCU or method that can be implemented.

 

Best answer by Jean-Christophe_TROTIN

Hi @inkong,

 

I think that the system that you described is possible with the STM32MP157 lines.

As you said that you “don’t know about MPU lines”, I could suggest that you have a look at the STM32 MPU wiki (https://wiki.st.com/stm32mpu/wiki/Main_Page), if you don’t know it yet.

 

The following articles might be interesting for you:

Hope this information helps.

 

Regards,

JC.

1 reply

Jean-Christophe_TROTIN
ST Employee
June 4, 2024

Hi @inkong,

 

I think that the system that you described is possible with the STM32MP157 lines.

As you said that you “don’t know about MPU lines”, I could suggest that you have a look at the STM32 MPU wiki (https://wiki.st.com/stm32mpu/wiki/Main_Page), if you don’t know it yet.

 

The following articles might be interesting for you:

Hope this information helps.

 

Regards,

JC.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
inkongAuthor
Associate
June 5, 2024

Hi Jean,

 

Thank you for your kind reply!! :)

I'll refer to the article you attached.

 

Sincerely,

inkong.