Skip to main content
Lead
April 2, 2024
Solved

Is there any Altium CircuitMaker project for the STM32MP series?

  • April 2, 2024
  • 1 reply
  • 1234 views

Hi!

I was recommended to use the pre-built basic start-up projects for the STM32MP series, instead of buildning my own from scratch.

Solved: Re: Why are the DDR_DQ signals mixed in unsorted o... - STMicroelectronics Community

The project files are Altium Designer only, and I have Altium CircuitMaker. Is there any way to export these files into Altium CircuitMaker?

 

 

Best answer by PatrickF

HI @DMårt 

sorry for late reply.

I have asked internally, but it seems complex to provide PCB exports of reference design as we cannot easily check on our side that the export was not introducing mistakes.

Anyway, the point is taken to check if we could enhance that in future (but nothing in short term).

Regards.

1 reply

PatrickF
PatrickFBest answer
Technical Moderator
May 24, 2024

HI @DMårt 

sorry for late reply.

I have asked internally, but it seems complex to provide PCB exports of reference design as we cannot easily check on our side that the export was not introducing mistakes.

Anyway, the point is taken to check if we could enhance that in future (but nothing in short term).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
DMårtAuthor
Lead
May 26, 2024

@PatrickF 

It's working to export from Altium Designer to CircuitMaker. No problem there. 

But I think CircuitMaker should be inclueded because CircuitMaker is very similar to Altium Designer. Almost copies. 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer