Skip to main content
OPetr.2
Associate II
November 3, 2023
Question

ISO7816 interface of STM32MP135 to connect SAM (Secure Module Access) Card

  • November 3, 2023
  • 1 reply
  • 1339 views

Hi

I see the STM32MP135 has an ISO7816 interface. Have you developed a compatible Linux device driver for the ISO7816 interface? There exist a software framework to use the SAM (Secure Module Access) Card connected to this interface?

Thank you,

This topic has been closed for replies.

1 reply

Bernard PUEL
Technical Moderator
November 7, 2023

ISO7816 is supported in UART STM32 driver from V5.0.0 release but there is no framework in Linux to use it.