Skip to main content
YRedd.2
Visitor II
June 7, 2023
Question

Issue running Hello world application

  • June 7, 2023
  • 1 reply
  • 973 views

Hi, I am using STM32MP157D-DK1 board to cross compile my application from host pc.

My host PC is installed with ubuntu 20.04. I have setup the build environment in host pc.

When i am executing the hello exe in STM32MP board.

Please find details below.

ubuntu_20_04@ubuntu2004:~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/hello$ uname -a

Linux ubuntu2004 5.4.0-42-generic #46-Ubuntu SMP Fri Jul 10 00:24:02 UTC 2020 x86_64 x86_64 x86_64 GNU/Linux

ubuntu_20_04@ubuntu2004:~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/hello$ lsb_release -a

No LSB modules are available.

Distributor ID:   Ubuntu

Description:   Ubuntu 20.04.1 LTS

Release:   20.04

Codename:   focal

ubuntu_20_04@ubuntu2004:~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/hello$ echo $CC

arm-ostl-linux-gnueabi-gcc -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a7 --sysroot=/home/ubuntu_20_04/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi

ubuntu_20_04@ubuntu2004:~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/hello$ echo $LD

arm-ostl-linux-gnueabi-ld --sysroot=/home/ubuntu_20_04/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi

ubuntu_20_04@ubuntu2004:~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/hello$ echo $LDFLAGS

-Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed

ubuntu_20_04@ubuntu2004:~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/hello$ echo $CFLAGS

-O2 -pipe -g -feliminate-unused-debug-types

ubuntu_20_04@ubuntu2004:~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/hello$ $CC hello.c -o hello_cc

ubuntu_20_04@ubuntu2004:~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/hello$ scp hello_cc root@192.168.7.15:/root/

hello_cc                                                                                                   100%  12KB  2.5MB/s  00:00   

ubuntu_20_04@ubuntu2004:~/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/hello$ ldd --version

ldd (Ubuntu GLIBC 2.31-0ubuntu9) 2.31

Copyright (C) 2020 Free Software Foundation, Inc.

This is free software; see the source for copying conditions. There is NO

warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

Written by Roland McGrath and Ulrich Drepper.

STM32MP OUTPUT:

./hello: /lib/libc.so.6 : version 'GLIBC-2.34' is not found (required by ./hello)

Please tell me how to resolve the issue. and also is there any procedure to develop code in STM cube IDE at host PC and then transferred into STM32MP board.

This topic has been closed for replies.

1 reply

Olivier GALLIEN
Technical Moderator
June 7, 2023

Hi @Yatam Venkata Krishna Reddy​ ,

Did you follow this article ?

Create a simple hello-world application - stm32mpu

Olivier

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.