Skip to main content
Associate II
September 18, 2024
Question

Issue with m4-native 1.4.18 Build on OpenSTLinux Dunfell

  • September 18, 2024
  • 1 reply
  • 935 views

We are working on building a gateway using the STM32MP1 and the RAK5146 concentrator module with the RAK5146 Pi Hat, utilizing the OpenSTLinux Dunfell distribution (v3.1.11).

While building the st-image-weston, we encountered an error during the compilation of m4-native-1.4.18. Below is a brief summary of the error:

ERROR: m4-native-1.4.18-r0 do_compile: oe_runmake failed

ERROR: Task (/.../m4-native_1.4.18.bb:do_compile) failed with exit code '1'

The reference used for integrating lorawan is https://wiki.st.com/stm32mpu-ecosystem-v3/wiki/How_to_integrate_LoRaWAN_gateway#ST_hardware

1 reply

Erwan SZYMANSKI
Technical Moderator
October 6, 2024

Hello @shreyaschandran ,
Yocto points you on which task fails and why does it fails here. So "m4-native" recipe cannot compile. You certainly have a longer error to explain where does the compilation fails and why.

Did you succeed to tackle this issue on your side ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.