Skip to main content
Associate II
October 30, 2023
Solved

Kernel stops loading in middle of boot-up

  • October 30, 2023
  • 1 reply
  • 1314 views

Hi there,

I have a custom board (with eMMC) that freezes in the middle of kernel loading:

Flyback_0-1698682455025.png

I am under the impression it is related with the rootfs.ext4, becuase it does not try the loading, but I am not sure yet.

Flash table is the following (I don´t use all the rest of partitions):

Flyback_1-1698682634773.png

Is there any way I can debug or any way to understand what is going on?

Thank you in advance.

This topic has been closed for replies.
Best answer by Flyback

Just in case somebody has the same issue, I was not pointing to the right partition in rootfs in extlinux.conf.

1 reply

FlybackAuthorBest answer
Associate II
October 31, 2023

Just in case somebody has the same issue, I was not pointing to the right partition in rootfs in extlinux.conf.