Skip to main content
Rc.1
Associate II
April 30, 2023
Question

MIPI display blank after enabling uart8

  • April 30, 2023
  • 1 reply
  • 1018 views

I'm using a custom stm32mp157a board with a DSI display.

If I enable uart8 using pins J8 (UART8_TX) and J9 (UART8_RX) the display driver (panel-sitronix-st7701.c) doesnt load properly and the display stays blank.

uart8 does work properly. If I disable uart8 the display works again.

This topic has been closed for replies.

1 reply

Kevin HUBER
Technical Moderator
May 2, 2023

Hello @Rc.1​ ,

Please can you share your complete boot log and your dtb file used.

Does the problem occurs only in Linux or directly from the boot?

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here