Skip to main content
Associate
October 2, 2025
Question

Optimize STM32MP135F RTC power consumption

  • October 2, 2025
  • 1 reply
  • 204 views

I have a STM32MP135F with a 3V3 47mF supercap on its VBAT line.

Internal RTC appears to work fine with power outages up to 3 or 4 hours, whereas I hoped one day.

 

I see in datasheet "Table 27. Current consumption in Vbat mode" that I can tweak VBAT powered sub-components to reduce this set (Backup SRAM, ) and increase RTC backup duration, but I fail to find those settings. Does anyone have it in mind?

 

I am using Yocto and OpenSTLinux on a board derived from DK2.

 

Regards

1 reply

PatrickF
Technical Moderator
October 2, 2025

Hi @aloiseau 

I think there is no DTS control for this. It is probably hardly coded inside TF-A or opTEE.
Look for PWR_CR2.BREN bit.

Regards

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
aloiseauAuthor
Associate
October 5, 2025

Thanks, guess I found it in optee-os-stm32mp recipe code, core/arch/arm/plat-stm32mp1/pm/low_power.c file, init_low_power function, alongside a "Keep backup RAM content in standby" comment. Will try and let you know!

 

By the way, but this is more a HW questions, my goal is to power RTC from VBAT and a small supercap. I also found PWR_CR2_MONEN bit I can disable to reduce VBAT power consumption (with related code within optee at least), and I guess I will need to look for LSE too, hoping it can be disabled to create a middle point between both first lines of datasheet table 27 (see after). Will see, did not dig yet, my hope is to go as low as 500nA despite datasheet which I hope do not reflect all possible combinaisons. If you have in mind another VBAT-powered line I should think about, I am interested :)

aloiseau_2-1759698304183.png

 

 

 

PatrickF
Technical Moderator
October 6, 2025

Hi @aloiseau 

stopping LSE is not possible as this is the clock for RTC.

Not possible to go in the 500nA range on STM32MP13 while keeping the RTC/LSE running.

So, either you put a larger supercap or you use an external RTC on I2C having extreme low power (like https://www.st.com/en/clocks-and-timers/m41t83.html), with 32khz feed to LSE (usually required for low power modes support by Linux). In that latter situation, VBAT of STM32MP13 could be connected to VDD.

Regards,

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here