Skip to main content
Associate II
July 22, 2025
Question

OSD32MP1-RED with kernel 6.6 failes to boot

  • July 22, 2025
  • 1 reply
  • 306 views

I'm trying to update linux kernel on OSD32MP1-RED board to the latest kernel 6.6.78 that's provided with Developer Package using instructions in README.HOW_TO.txt.stm32mp1, but after building and installing kernel and modules on SD card booting from  SD card hangs and then board goes into continuous cycle of rebooting due to watchdog. Is there a way to use latest ST kernel with this board? Here is output from the booting:


NOTICE: CPU: STM32MP157F?? Rev.Z
NOTICE: Model: Octavo OSD32MP1 RED board
INFO: Reset reason (0x214):
INFO: IWDG2 Reset (rst_iwdg2)
INFO: PMIC version = 0x21
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):v2.4-stm32mp-r1
NOTICE: BL2: Built : 23:04:23, Apr 24 2022
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
WARNING: Couldn't find property st,phy-cal in dtb
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff226
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc5000
INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd847c
WARNING: Not a known TEE, use default loading options.
INFO: BL2: Skip loading image id 21
INFO: BL2: Skip loading image id 22
INFO: BL2: Loading image id 23
INFO: Loading image id=23 at address 0xc0500000
INFO: Image id=23 loaded: 0xc0500000 - 0xc0514c5b
INFO: BL2: Loading image id 26
INFO: Loading image id=26 at address 0x2ffc0000
INFO: Image id=26 loaded: 0x2ffc0000 - 0x2ffc401c
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01cf910
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc5000
INFO: SPSR = 0x1d3
NOTICE: SP_MIN: v2.4-r1.0(debug):v2.4-stm32mp-r1
NOTICE: SP_MIN: Built : 23:04:26, Apr 24 2022
INFO: ARM GICv2 driver initialized
INFO: Set calibration timer to 60 sec
INFO: stm32mp1 IWDG1 is secure
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world


U-Boot 2020.10-stm32mp-r1 (Apr 24 2022 - 23:05:27 +0000)

CPU: STM32MP157F?? Rev.Z
Model: Octavo OSD32MP1 RED board
Board: stm32mp1 in trusted mode (st,stm32mp157c-osd32mp1-red)
DRAM: 512 MiB
Clocks:
- MPU : 650 MHz
- MCU : 187.500 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1
Loading Environment from MMC... OK
In: serial
Out: serial
Err: serial
invalid MAC address in OTP 00:00:00:00:00:00
Net:
Error: ethernet@5800a000 address not set.
No ethernet found.

Hit any key to stop autoboot: 0
Boot over mmc0!
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:4...
Found /mmc0_extlinux/extlinux.conf
Retrieving file: /mmc0_extlinux/extlinux.conf
363 bytes read in 24 ms (14.6 KiB/s)
Retrieving file: /splash.bmp
170122 bytes read in 31 ms (5.2 MiB/s)
1: osd32mp1-red-sdcard
Retrieving file: /uImage
8787720 bytes read in 396 ms (21.2 MiB/s)
append: root=/dev/mmcblk1p6 rootwait rw console=ttySTM0,115200 init=/sbin/init firmware_class/
Retrieving file: /stm32mp157c-osd32mp1-red.dtb
62249 bytes read in 27 ms (2.2 MiB/s)
## Booting kernel from Legacy Image at c2000000 ...
Image Name: Linux-6.6.78
Created: 2025-07-16 18:57:16 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 8787656 Bytes = 8.4 MiB
Load Address: c2000040
Entry Point: c2000040
Verifying Checksum ... OK
## Flattened Device Tree blob at c4000000
Booting using the fdt blob at 0xc4000000
XIP Kernel Image
Loading Device Tree to cffed000, end cffff328 ... OK

Starting kernel ...

INFO: CPU 0 IT Watchdog 2
INFO: CPU : 0
INFO: sp_usr : 0x0
INFO: lr_usr : 0x0

1 reply

Olivier GALLIEN
Technical Moderator
July 22, 2025

Hi @DevESG 

 

I notice you are using TF-A v2.4-stm32mp-r1 U-Boot 2020.10-stm32mp-r1 which are former version from OSTL 3.1 now deprecated. 

Kernel 6.6.78 can only be installed on top of consistent BSP from compatible OSTL 6.1. 

TF-A v2.10-stm32mp-r2

U-Boot v2023.10-stm32mp-r2

OP-TEE v4.0.0-stm32mp-r2 

Octavo support might probably provide them for OSD32MP1-RED or help you to migrate.  

Olivier 

 

 

 

 

 

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
DevESGAuthor
Associate II
July 22, 2025

Thanks Olivier, as you suggested I'll try to contact octavo support about possibility to update packages you mentioned to support OSD32MP1-RED board.

Ivan