Skip to main content
wG.1
Associate II
March 13, 2024
Solved

run Weston fail on Buildroot

  • March 13, 2024
  • 1 reply
  • 2374 views

 

Hi,

The MP157F-DK2 comes with an SD card attached. Weston (ver 5.0.0) with DRM works well.
But if I want to run Weston(ver 10.0.1) on Buildroot, it will fail.

Do I need to build more packages for Weston?

I am using the version of Buildroot.

a. buildroot: remotes/origin/st/2023.02.6
b. buildroot-external-st: remotes/origin/st/2023.02.2

 

This is the failure log, and the attachment is the success log of the SD card that comes with the MP157F-DK2.

# export XDG_RUNTIME_DIR=/run/user/root
# mkdir --parents $XDG_RUNTIME_DIR
# chmod 0700 $XDG_RUNTIME_DIR

# weston --tty=1
[00:01:34.112] weston 10.0.1
 https://wayland.freedesktop.org
 Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
 Build: 2021.05-10575-gae4a6e0c24
[00:01:34.113] Command line: weston --tty=1
[00:01:34.113] OS: Linux, 6.1.28, #1 SMP PREEMPT Tue Feb 20 15:20:37 CST 2024, armv7l
[00:01:34.113] Flight recorder: enabled
[00:01:34.113] Starting with no config file.
[00:01:34.114] Output repaint window is 7 ms maximum.
[00:01:34.114] Loading module '/usr/lib/libweston-10/drm-backend.so'
[00:01:34.118] initializing drm backend
[00:01:34.118] Trying weston_launch launcher...
[00:01:34.118] could not get launcher fd from env
[00:01:34.118] Trying direct launcher...
[00:01:34.123] using /dev/dri/card0
[00:01:34.123] DRM: supports atomic modesetting
[00:01:34.123] DRM: supports GBM modifiers
[00:01:34.123] DRM: supports picture aspect ratio
[00:01:34.123] Compiled without GBM/EGL support
[00:01:34.123] failed to initialize egl
[00:01:34.123] fatal: failed to create compositor backend

 

Would you give an advice?

Thanks for reading.

 

This topic has been closed for replies.
Best answer by Kevin HUBER

Hello @wG.1 ,

 

For question specific to buildroot, it is recommended to contact our partner that support buildroot on our STM32MP1 platforms:

https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ecosystem_release_note_-_v5.0.0#Buildroot_-28Arm-C2-AE_Cortex-C2-AE-A7-29

 

Bootlin has developed specific support, demonstration configurations and documentation to help ST customers use Buildroot on STM32MP1 platforms.
 

See https://www.st.com/content/st_com/en/partner/partner-program/partnerpage/Bootlin.html
To address Bootlin technical support: buildroot-st-support@bootlin.com

Hope it helps,

Best Regards,

Kevin

1 reply

Kevin HUBER
Kevin HUBERBest answer
Technical Moderator
April 9, 2024

Hello @wG.1 ,

 

For question specific to buildroot, it is recommended to contact our partner that support buildroot on our STM32MP1 platforms:

https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ecosystem_release_note_-_v5.0.0#Buildroot_-28Arm-C2-AE_Cortex-C2-AE-A7-29

 

Bootlin has developed specific support, demonstration configurations and documentation to help ST customers use Buildroot on STM32MP1 platforms.
 

See https://www.st.com/content/st_com/en/partner/partner-program/partnerpage/Bootlin.html
To address Bootlin technical support: buildroot-st-support@bootlin.com

Hope it helps,

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here