Skip to main content
Associate II
March 12, 2025
Question

scarthgap STM32MP157 PMIC no DDR VDD (buck2) output

  • March 12, 2025
  • 1 reply
  • 582 views

Hello

I have a cutom board based on STM32MP157D-EV1.

The dts is based on stm32mp157f-ed1.dts with minor differences:

* HSE: Bypass -> crystal (There is a 24MHz crystal). Removed "st,digbypass;" from &clk_hse

* DDR: 32bit 8Gb -> 16bit 4Gb. (Using MT41K256M16TW-107). Change the included ddr.dtsi to #include "stm32mp15-ddr3-1x4Gb-1066-binG.dtsi"

 

When flashing, I get this error: ERROR: DDR addr bus test: can't access memory @ 0xc0000004

I can see that the 1.35V does never ouput from BUCK2 of the PMIC, so I assume that the origin of the issue is there. I have modified the tf-a code to add traces and can see that buck2 should indeed be enabled. 

The HW works: I have run another build based on kirkstone on the same HW.

 

I am running out of ideas of where to look next. Does anyone have any ideas?

 

The dts:

 

Spoiler
// SPDX-License-Identifier: (GPL-2.0-or-later OR BSD-3-Clause)
/*
 * Copyright (C) STMicroelectronics 2022 - All Rights Reserved
 * Author: Alexandre Torgue <alexandre.torgue@foss.st.com> for STMicroelectronics.
 */
/dts-v1/;

#include "stm32mp157.dtsi"
#include "stm32mp15xd.dtsi"
#include "stm32mp15-pinctrl.dtsi"
#include "stm32mp15xxaa-pinctrl.dtsi"
#include <dt-bindings/clock/stm32mp1-clksrc.h>
#include "stm32mp15-ddr3-1x4Gb-1066-binG.dtsi"

/ {
	model = "STMicroelectronics STM32MP157D XXX";
	compatible = "st,stm32mp157d-ed1", "st,stm32mp157";

	chosen {
		stdout-path = "serial0:115200n8";
	};

	memory@c0000000 {
		device_type = "memory";
		reg = <0xC0000000 0x20000000>;
	};

	aliases {
		serial0 = &uart4;
	};
};

&bsec {
	board_id: board_id@ec {
		reg = <0xec 0x4>;
		st,non-secure-otp;
	};
};

&clk_hse {
	
};

&cpu0 {
	cpu-supply = <&vddcore>;
};

&cpu1 {
	cpu-supply = <&vddcore>;
};

&ddr {
	vdd-supply = <&vdd_ddr>;
	vtt-supply = <&vtt_ddr>;
	vref-supply = <&vref_ddr>;
};

&fmc {
	pinctrl-names = "default";
	pinctrl-0 = <&fmc_pins_a>;
	status = "okay";

	nand-controller@4,0 {
		status = "okay";

		nand@0 {
			reg = <0>;
			nand-on-flash-bbt;
			#address-cells = <1>;
			#size-cells = <1>;
		};
	};
};

&hash1 {
	status = "okay";
};

&i2c4 {
	pinctrl-names = "default";
	pinctrl-0 = <&i2c4_pins_a>;
	i2c-scl-rising-time-ns = <185>;
	i2c-scl-falling-time-ns = <20>;
	clock-frequency = <400000>;
	status = "okay";

	pmic: stpmic@33 {
		compatible = "st,stpmic1";
		reg = <0x33>;
		interrupts-extended = <&exti_pwr 55 IRQ_TYPE_EDGE_FALLING>;
		interrupt-controller;
		#interrupt-cells = <2>;
		status = "okay";

		regulators {
			compatible = "st,stpmic1-regulators";
			ldo1-supply = <&v3v3>;
			ldo2-supply = <&v3v3>;
			ldo3-supply = <&vdd_ddr>;
			ldo5-supply = <&v3v3>;
			ldo6-supply = <&v3v3>;
			pwr_sw1-supply = <&bst_out>;
			pwr_sw2-supply = <&bst_out>;

			vddcore: buck1 {
				regulator-name = "vddcore";
				regulator-min-microvolt = <1200000>;
				regulator-max-microvolt = <1350000>;
				regulator-always-on;
				regulator-initial-mode = <0>;
				regulator-over-current-protection;
			};

			vdd_ddr: buck2 {
				regulator-name = "vdd_ddr";
				regulator-min-microvolt = <1350000>;
				regulator-max-microvolt = <1350000>;
				regulator-always-on;
				regulator-initial-mode = <0>;
				regulator-over-current-protection;
			};

			vdd: buck3 {
				regulator-name = "vdd";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
				st,mask-reset;
				regulator-initial-mode = <0>;
				regulator-over-current-protection;
			};

			v3v3: buck4 {
				regulator-name = "v3v3";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
				regulator-over-current-protection;
				regulator-initial-mode = <0>;
			};

			vdda: ldo1 {
				regulator-name = "vdda";
				regulator-min-microvolt = <2900000>;
				regulator-max-microvolt = <2900000>;
			};

			v2v8: ldo2 {
				regulator-name = "v2v8";
				regulator-min-microvolt = <2800000>;
				regulator-max-microvolt = <2800000>;
			};

			vtt_ddr: ldo3 {
				regulator-name = "vtt_ddr";
				regulator-always-on;
				regulator-over-current-protection;
				st,regulator-sink-source;
			};

			vdd_usb: ldo4 {
				regulator-name = "vdd_usb";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
			};

			vdd_sd: ldo5 {
				regulator-name = "vdd_sd";
				regulator-min-microvolt = <2900000>;
				regulator-max-microvolt = <2900000>;
				regulator-boot-on;
			};

			v1v8: ldo6 {
				regulator-name = "v1v8";
				regulator-min-microvolt = <1800000>;
				regulator-max-microvolt = <1800000>;
			};

			vref_ddr: vref_ddr {
				regulator-name = "vref_ddr";
				regulator-always-on;
			};

			bst_out: boost {
				regulator-name = "bst_out";
			};

			vbus_otg: pwr_sw1 {
				regulator-name = "vbus_otg";
			};

			vbus_sw: pwr_sw2 {
				regulator-name = "vbus_sw";
				regulator-active-discharge = <1>;
			};
		};
	};
};

&iwdg1 {
	timeout-sec = <32>;
	status = "okay";
};

&pwr_regulators {
	vdd-supply = <&vdd>;
	vdd_3v3_usbfs-supply = <&vdd_usb>;
};



&qspi {
	pinctrl-names = "default";
	pinctrl-0 = <&qspi_clk_pins_a &qspi_bk1_pins_a>;
	reg = <0x58003000 0x1000>, <0x70000000 0x4000000>;
	#address-cells = <1>;
	#size-cells = <0>;
	status = "okay";

	flash0: mx66l51235l@0 {
		compatible = "jedec,spi-nor";
		reg = <0>;
		spi-rx-bus-width = <4>;
		spi-max-frequency = <108000000>;
		#address-cells = <1>;
		#size-cells = <1>;
	};
};

&rcc {
	compatible = "st,stm32mp1-rcc-secure", "st,stm32mp1-rcc", "syscon";
	st,clksrc=<
		CLK_MPU_PLL1P
		CLK_AXI_PLL2P
		CLK_MCU_PLL3P
		CLK_MCO1_DISABLED
		CLK_MCO2_DISABLED
		CLK_CKPER_HSE
		CLK_FMC_ACLK
		CLK_QSPI_ACLK
		CLK_ETH_PLL4P
		CLK_SDMMC12_PLL4P
		CLK_DSI_DSIPLL
		CLK_STGEN_HSE
		CLK_USBPHY_HSE
		CLK_SPI2S1_PLL3Q
		CLK_SPI2S23_PLL3Q
		CLK_SPI45_HSI
		CLK_SPI6_HSI
		CLK_I2C46_HSI
		CLK_SDMMC3_PLL4P
		CLK_USBO_USBPHY
		CLK_ADC_CKPER
		CLK_CEC_LSE
		CLK_I2C12_HSI
		CLK_I2C35_HSI
		CLK_UART1_HSI
		CLK_UART24_HSI
		CLK_UART35_HSI
		CLK_UART6_HSI
		CLK_UART78_HSI
		CLK_SPDIF_PLL4P
		CLK_FDCAN_PLL4R
		CLK_SAI1_PLL3Q
		CLK_SAI2_PLL3Q
		CLK_SAI3_PLL3Q
		CLK_SAI4_PLL3Q
		CLK_RNG1_CSI
		CLK_RNG2_LSI
		CLK_LPTIM1_PCLK1
		CLK_LPTIM23_PCLK3
		CLK_LPTIM45_LSE
	>;

	st,clkdiv = <
		DIV(DIV_MPU, 1)
		DIV(DIV_AXI, 0)
		DIV(DIV_MCU, 0)
		DIV(DIV_APB1, 1)
		DIV(DIV_APB2, 1)
		DIV(DIV_APB3, 1)
		DIV(DIV_APB4, 1)
		DIV(DIV_APB5, 2)
		DIV(DIV_MCO1, 0)
		DIV(DIV_MCO2, 0)
	>;

	st,pll_vco {
		pll2_vco_1066Mhz: pll2-vco-1066Mhz {
			src=<CLK_PLL12_HSE>;
			divmn = <2 65>;
			frac = <0x1400>;
		};

		pll3_vco_417Mhz: pll3-vco-417Mhz {
			src=<CLK_PLL3_HSE>;
			divmn = <1 33>;
			frac = <0x1a04>;
		};

		pll4_vco_594Mhz: pll4-vco-594Mhz {
			src=<CLK_PLL4_HSE>;
			divmn = <3 98>;
		};
	};

	/* VCO = 1066.0 MHz => P = 266 (AXI), Q = 533 (GPU), R = 533 (DDR) */
	pll2: st,pll@1 {
		compatible = "st,stm32mp1-pll";
		reg = <1>;

		st,pll = <&pll2_cfg1>;

		pll2_cfg1: pll2_cfg1 {
			st,pll_vco = <&pll2_vco_1066Mhz>;
			st,pll_div_pqr = <1 0 0>;
		};
	};

	/* VCO = 417.8 MHz => P = 209, Q = 24, R = 11 */
	pll3: st,pll@2 {
		compatible = "st,stm32mp1-pll";
		reg = <2>;

		st,pll = <&pll3_cfg1>;

		pll3_cfg1: pll3_cfg1 {
			st,pll_vco = <&pll3_vco_417Mhz>;
			st,pll_div_pqr = <1 16 36>;
		};
	};

	/* VCO = 594.0 MHz => P = 99, Q = 74, R = 74 */
	pll4: st,pll@3 {
		compatible = "st,stm32mp1-pll";
		reg = <3>;

		st,pll = <&pll4_cfg1>;

		pll4_cfg1: pll4_cfg1 {
			st,pll_vco = <&pll4_vco_594Mhz>;
			st,pll_div_pqr = <5 7 7>;
		};
	};
};

&rng1 {
	status = "okay";
};

&rtc {
	status = "okay";
};

&sdmmc1 {
	pinctrl-names = "default";
	pinctrl-0 = <&sdmmc1_b4_pins_a &sdmmc1_dir_pins_a>;
	disable-wp;
	st,sig-dir;
	st,neg-edge;
	st,use-ckin;
	bus-width = <4>;
	vmmc-supply = <&vdd_sd>;
	sd-uhs-sdr12;
	sd-uhs-sdr25;
	sd-uhs-sdr50;
	sd-uhs-ddr50;
	status = "okay";
};

&sdmmc2 {
	pinctrl-names = "default";
	pinctrl-0 = <&sdmmc2_b4_pins_a &sdmmc2_d47_pins_a>;
	non-removable;
	no-sd;
	no-sdio;
	st,neg-edge;
	bus-width = <8>;
	vmmc-supply = <&v3v3>;
	vqmmc-supply = <&vdd>;
	mmc-ddr-3_3v;
	status = "okay";
};

&uart4 {
	pinctrl-names = "default";
	pinctrl-0 = <&uart4_pins_a>;
	status = "okay";
};

 

1 reply

MakandraAuthor
Associate II
March 13, 2025

Hello

I found a way forward:

In stm32mp_pmic.c,

void initialize_pmic(void)
{
	
	if (!initialize_pmic_i2c()) {
		VERBOSE("No PMIC\n");
		return;
	}

	register_pmic_shared_peripherals();

	if (register_pmic() < 0) {
		panic();
	}

//Remove these lines and buck2 will enable the output
//if (stpmic1_powerctrl_on() < 0) {
//		panic();
//	}
	
}

 

I did not make up the solution, I found it from an inherited project. Does anyone have any explaination to why this works?