Skip to main content
Associate III
June 26, 2025
Question

st-stm32mp-tsn-swch Persistent self configured IP address

  • June 26, 2025
  • 1 reply
  • 624 views

Can I only modify the ttt-ip-init-systemd.sh script if I need to change and persist the IP address while using the STM32MP switch mode?

bugman_0-1750906748881.png

 

1 reply

Bernard PUEL
Technical Moderator
June 27, 2025

YEs the script is there for that so you can customize it for your setup or product !

bugmanAuthor
Associate III
July 1, 2025

Can I use the service in Systemd to set it up?

Bernard PUEL
Technical Moderator
July 4, 2025

Of course you can. 

As soon as the switch driver is probed, the configuration is done by Kernel standard interfaces.