Skip to main content
Associate II
August 3, 2023
Solved

STLINK-V3MODS for STM32MP1 Compatibility

  • August 3, 2023
  • 2 replies
  • 1709 views

Hello,

I am in process of designing my own STM32MP1 powered device. I was wondering if I can use STLINK-V3MODS as a drop in replacement for ST-LINK/V2-1 in STM32MP157-EVAL reference design. I need the Virtual COM interface embedded in device.

-Mark

This topic has been closed for replies.
Best answer by PatrickF

Hi @mhd0425 

Although I guess STLINK-V3MODS has not been specifically tested on STM32MP1 devices, all STLINKs flavors are compatible with STM32MP1 (assuming VDD=3.3V).

If you are interested only in Virtual Com Port, and depending on amount of product you will product, maybe there could be some cheaper solutions:

  • use a cheap STM32 part to do only UART/USB bridge (I guess USB full-speed would be enough for VCP)
  • use a dedicated UART/USB bridge component or cable (e.g. FTDI chips/cables)

For debugging, providing an STDC14 (or other) connector on your board would allows to use any external debuggers (STLINK or other) during development phase.

Regards.

2 replies

PatrickF
PatrickFBest answer
Technical Moderator
August 4, 2023

Hi @mhd0425 

Although I guess STLINK-V3MODS has not been specifically tested on STM32MP1 devices, all STLINKs flavors are compatible with STM32MP1 (assuming VDD=3.3V).

If you are interested only in Virtual Com Port, and depending on amount of product you will product, maybe there could be some cheaper solutions:

  • use a cheap STM32 part to do only UART/USB bridge (I guess USB full-speed would be enough for VCP)
  • use a dedicated UART/USB bridge component or cable (e.g. FTDI chips/cables)

For debugging, providing an STDC14 (or other) connector on your board would allows to use any external debuggers (STLINK or other) during development phase.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
mhd0425Author
Associate II
August 7, 2023

Thank you @PatrickF this is exactly what I needed.

By the way, "Email me when someone replies" did not seem to work..