STM32MP1 + STPMIC1A PMIC Power issue
- September 6, 2023
- 2 replies
- 3239 views
Hi ~
I am using STM32MP157C MPU + STPMIC1A for my custom board with ecosystem 4.1
And unfortunately I'm wrestling with some problem regarding PMIC.
I produced 30 boards for sample.
Some board is working fine but some board has power issue.
1) Custom board configuration
My custom board consists of a CPU and BASE board like EV1 Evaluation board.
CPU board has STM32MP157C MPU + STPMIC1A + DDR, eMMC.
Base board has various peripheral such as USB, I/O, HDMI, microSD and so on.
2) PMIC issue
Boot device is eMMC (SDINBDG4-16G-XI1).
STPMIC1A BUCK4's default output level is 3.3V and eMMC use it for VCC.
In some boards without any problem, BUCK4 output 3.3V normally.
In some boards with the problem, BUCK4 output 3.17V abnormally.
Plus, it looks like as following with a cycle time of about 250ms,
As a result, the board fails to boot.
Yellow is 5VIN and Blue is BUCK4 output.


3) VIN Threshold
The first is a picture of a normal board and
the second is a picture of an abnormal board.


4) Others
All the pictures above were tested with the CPU board only, without the base board.
If I connect the BASE board, the BUCK4 voltage level drops to 1.78V.
I attached my schematics.
Please tell me if there are something I should check.
Thank you
Best regards