Skip to main content
Associate II
March 18, 2025
Question

STM32MP135D-ODYSSEY booting gets struck with INFO: SPSR = 0x1d3 message after BL2 booting BL32 with SD Card

  • March 18, 2025
  • 1 reply
  • 700 views

aravindhan:~$ sudo picocom -b 115200 /dev/ttyUSB0
picocom v3.1

port is : /dev/ttyUSB0
flowcontrol : none
baudrate is : 115200
parity is : none
databits are : 8
stopbits are : 1
escape is : C-a
local echo is : no
noinit is : no
noreset is : no
hangup is : no
nolock is : no
send_cmd is : sz -vv
receive_cmd is : rz -vv -E
imap is :
omap is :
emap is : crcrlf,delbs,
logfile is : none
initstring : none
exit_after is : not set
exit is : no

Type [C-a] [C-h] to see available commands
Terminal ready
�NOTICE: CPU: STM32MP135D Rev.Y
NOTICE: Model: Seeed STM32MP135D Odyssey Board
INFO: PMIC version = 0x21
INFO: Reset reason (0x35):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe0000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r1.0(debug):38df888b0-dirty(38df888b)
NOTICE: BL2: Built : 01:36:41, Mar 15 2024
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-1066 bin F 1x4Gb 533MHz v1.53
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x30006000
INFO: Image id=1 loaded: 0x30006000 - 0x30006246
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x30006000
INFO: FCONF: Reading firmware configuration information for: mce_config
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0xde200000
INFO: Image id=4 loaded: 0xde200000 - 0xde20001c
INFO: OPTEE ep=0xde200000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0xde200000
INFO: Image id=8 loaded: 0xde200000 - 0xde277418
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0400000
INFO: Image id=2 loaded: 0xc0400000 - 0xc040e648
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0000000
INFO: Image id=5 loaded: 0xc0000000 - 0xc0115bd8
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0xde200000
INFO: SPSR = 0x1d3                                                            ---- here fw-config is disabled in tf-a and I changed OP-TEE header address (init_load_addr) in /build-openstlinuxweston-stm32mp1/workspace/sources/tf-a-stm32mp/lib/optee/optee_utils.c to bypass my previous error "WARNING: The load address in optee header 0xde000000 - 0xde077418 is not in reserved area: 0xde200000 - 0xe0000000.
ERROR: OPTEE header parse error."

1 reply

ST Employee
March 27, 2025

Hi @aravindhan,

 

Could you share your U-boot device tree with me and explain a little more about what you want to do?

 

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
March 27, 2025

I notice in my plat-stm32mp1/conf.mk file that for stm32mp13  

CFG_STM32MP_PROFILE ?= secure_and_system_services, so this means it will be running in SYSRAM right? but after that it forces to use DDR (
$(call force,CFG_STM32MP1_OPTEE_IN_SYSRAM,n)
) why? I will also attach my conf.mk and U-boot device tree file below.----------------------------------------------------------------
# 1GB and 512MB DDR targets do not locate secure DDR at the same place.
flavor_dts_file-157A_DHCOR_AVENGER96 = stm32mp157a-dhcor-avenger96.dts
flavor_dts_file-157A_DK1 = stm32mp157a-dk1.dts
flavor_dts_file-157A_ED1 = stm32mp157a-ed1.dts
flavor_dts_file-157A_EV1 = stm32mp157a-ev1.dts
flavor_dts_file-157C_DHCOM_PDK2 = stm32mp157c-dhcom-pdk2.dts
flavor_dts_file-157C_DK2 = stm32mp157c-dk2.dts
flavor_dts_file-157C_ED1 = stm32mp157c-ed1.dts
flavor_dts_file-157C_EV1 = stm32mp157c-ev1.dts
flavor_dts_file-157D_DK1 = stm32mp157d-dk1.dts
flavor_dts_file-157D_ED1 = stm32mp157d-ed1.dts
flavor_dts_file-157D_EV1 = stm32mp157d-ev1.dts
flavor_dts_file-157F_DK2 = stm32mp157f-dk2.dts
flavor_dts_file-157F_ED1 = stm32mp157f-ed1.dts
flavor_dts_file-157F_EV1 = stm32mp157f-ev1.dts

flavor_dts_file-135F_DK = stm32mp135f-dk.dts
flavor_dts_file-135D_ODYSSEY = stm32mp135d-odyssey.dts

flavorlist-cryp-512M = $(flavor_dts_file-157C_DK2) \
$(flavor_dts_file-157F_DK2) \
$(flavor_dts_file-135F_DK) \
$(flavor_dts_file-135D_ODYSSEY)

flavorlist-no_cryp-512M = $(flavor_dts_file-157A_DK1) \
$(flavor_dts_file-157D_DK1)

flavorlist-cryp-1G = $(flavor_dts_file-157C_DHCOM_PDK2) \
$(flavor_dts_file-157C_ED1) \
$(flavor_dts_file-157C_EV1) \
$(flavor_dts_file-157F_ED1) \
$(flavor_dts_file-157F_EV1)

flavorlist-no_cryp-1G = $(flavor_dts_file-157A_ED1) \
$(flavor_dts_file-157A_EV1) \
$(flavor_dts_file-157A_DHCOR_AVENGER96) \
$(flavor_dts_file-157D_ED1) \
$(flavor_dts_file-157D_EV1)

flavorlist-no_cryp = $(flavorlist-no_cryp-512M) \
$(flavorlist-no_cryp-1G)

flavorlist-512M = $(flavorlist-cryp-512M) \
$(flavorlist-no_cryp-512M)

flavorlist-1G = $(flavorlist-cryp-1G) \
$(flavorlist-no_cryp-1G)

flavorlist-MP15 = $(flavor_dts_file-157A_DHCOR_AVENGER96) \
$(flavor_dts_file-157A_DK1) \
$(flavor_dts_file-157A_ED1) \
$(flavor_dts_file-157A_EV1) \
$(flavor_dts_file-157C_DHCOM_PDK2) \
$(flavor_dts_file-157C_DK2) \
$(flavor_dts_file-157C_ED1) \
$(flavor_dts_file-157C_EV1) \
$(flavor_dts_file-157D_DK1) \
$(flavor_dts_file-157D_ED1) \
$(flavor_dts_file-157D_EV1) \
$(flavor_dts_file-157F_DK2) \
$(flavor_dts_file-157F_ED1) \
$(flavor_dts_file-157F_EV1)

#flavorlist-MP13 = $(flavor_dts_file-135F_DK)
flavorlist-MP13 = $(flavor_dts_file-135D_ODYSSEY)

# External device tree default path
CFG_EXT_DTS ?= $(arch-dir)/dts/external-dt/optee

# Extend flavorlists with external device trees
ifneq ($(wildcard $(CFG_EXT_DTS)/conf.mk),)
-include $(CFG_EXT_DTS)/conf.mk
endif

# List of all DTS for this PLATFORM
ALL_DTS = $(flavorlist-MP15) $(flavorlist-MP13)

# Check if device-tree exist in OP-TEE source code, else search it in external
# device tree repository
ifeq ($(wildcard $(arch-dir)/dts/$(CFG_EMBED_DTB_SOURCE_FILE)),)
ifneq ($(wildcard $(CFG_EXT_DTS)/$(CFG_EMBED_DTB_SOURCE_FILE)),)
override dts-source-path := $(CFG_EXT_DTS)
else
$(error Cannot find DTS file $(CFG_EXT_DTS)/$(CFG_EMBED_DTB_SOURCE_FILE))
endif
endif

ifneq ($(PLATFORM_FLAVOR),)
ifeq ($(flavor_dts_file-$(PLATFORM_FLAVOR)),)
$(error Invalid platform flavor $(PLATFORM_FLAVOR))
endif
CFG_EMBED_DTB_SOURCE_FILE ?= $(flavor_dts_file-$(PLATFORM_FLAVOR))
endif
CFG_EMBED_DTB_SOURCE_FILE ?= stm32mp157c-dk2.dts

# CFG_STM32MP1x switches are exclusive.
# - CFG_STM32MP15 is enabled for STM32MP15x-* targets (default)
# - CFG_STM32MP13 is enabled for STM32MP13x-* targets
# We try to guess the variant from the embedded DT source file name
ifneq ($(filter $(CFG_EMBED_DTB_SOURCE_FILE),$(flavorlist-MP13)),)
$(call force,CFG_STM32MP13,y)
endif
ifneq ($(filter $(CFG_EMBED_DTB_SOURCE_FILE),$(flavorlist-MP15)),)
$(call force,CFG_STM32MP15,y)
endif

ifeq ($(CFG_STM32MP13),y)
$(call force,CFG_STM32MP15,n)
else
$(call force,CFG_STM32MP15,y)
$(call force,CFG_STM32MP13,n)
endif

ifeq ($(call cfg-one-enabled,CFG_STM32MP15 CFG_STM32MP13),n)
$(error One of CFG_STM32MP15 CFG_STM32MP13 must be enabled)
endif
ifeq ($(call cfg-all-enabled,CFG_STM32MP15 CFG_STM32MP13),y)
$(error Only one of CFG_STM32MP15 CFG_STM32MP13 must be enabled)
endif

# CFG_STM32MP_PROFILE selects the profile of the services embedded
# in OP-TEE.

ifeq ($(CFG_STM32MP13),y)
# STM32MP13: default select secure_and_system_services.
# Alternate system_services is supported.
CFG_STM32MP_PROFILE ?= secure_and_system_services
endif #CFG_STM32MP13

ifeq ($(CFG_STM32MP15),y)
# STM32MP15: default select system_services, OP-TEE executes in DDR
# (i.e. CFG_STM32MP1_OPTEE_IN_SYSRAM=n).
# Alternate secure_and_system_services executes in SRAM
# (i.e. CFG_STM32MP1_OPTEE_IN_SYSRAM=y).
ifeq ($(CFG_STM32MP1_OPTEE_IN_SYSRAM),y)
$(call force,CFG_STM32MP_PROFILE,secure_and_system_services)
endif
CFG_STM32MP_PROFILE ?= system_services
ifeq ($(CFG_STM32MP_PROFILE),secure_and_system_services)
$(call force,CFG_STM32MP1_OPTEE_IN_SYSRAM,y,Required by secure_and_system_services profile)
else
$(call force,CFG_STM32MP1_OPTEE_IN_SYSRAM,n,Required by system_services profile)
endif
endif #CFG_STM32MP15

ifeq ($(filter $(CFG_STM32MP_PROFILE),system_services secure_and_system_services),)
$(error CFG_STM32MP_PROFILE shall be one of system_services or secure_and_system_services)
endif

ifeq ($(CFG_STM32MP_PROFILE),system_services)
include $(platform-dir)/conf.disable-secure-services.mk
endif

ifneq ($(filter $(CFG_EMBED_DTB_SOURCE_FILE),$(flavorlist-no_cryp)),)
$(call force,CFG_STM32_CRYP,n)
$(call force,CFG_STM32_PKA,n)
$(call force,CFG_STM32_SAES,n)
endif

ifneq ($(filter $(CFG_EMBED_DTB_SOURCE_FILE),$(flavorlist-no_rng)),)
$(call force,CFG_HWRNG_PTA,n)
$(call force,CFG_STM32_PKA,n)
$(call force,CFG_STM32_SAES,n)
CFG_WITH_SOFTWARE_PRNG ?= y
endif

# Default do not access external DT passed to non-secure boot stage
CFG_EXTERNAL_DT ?= n

include core/arch/arm/cpu/cortex-a7.mk

$(call force,CFG_ARM_GIC_PM,y)
$(call force,CFG_DRIVERS_CLK,y)
$(call force,CFG_DRIVERS_CLK_DT,y)
$(call force,CFG_DRIVERS_GPIO,y)
$(call force,CFG_DRIVERS_PINCTRL,y)
$(call force,CFG_DRIVERS_REGULATOR,y)
$(call force,CFG_GIC,y)
$(call force,CFG_INIT_CNTVOFF,y)
$(call force,CFG_PM_ARM32,y)
$(call force,CFG_PSCI_ARM32,y)
$(call force,CFG_REGULATOR_FIXED,y)
$(call force,CFG_SECURE_TIME_SOURCE_CNTPCT,y)
$(call force,CFG_SM_PLATFORM_HANDLER,y)
$(call force,CFG_STM32_SHARED_IO,y)

ifeq ($(CFG_STM32MP13),y)
$(call force,CFG_BOOT_SECONDARY_REQUEST,n)
$(call force,CFG_CORE_ASYNC_NOTIF,y)
$(call force,CFG_CORE_ASYNC_NOTIF_GIC_INTID,31)
$(call force,CFG_CORE_RESERVED_SHM,n)
$(call force,CFG_DRIVERS_ADC,y)
$(call force,CFG_DRIVERS_CLK,y)
$(call force,CFG_DRIVERS_CLK_FIXED,y)
$(call force,CFG_SCMI_MSG_PERF_DOMAIN,y)
$(call force,CFG_SECONDARY_INIT_CNTFRQ,n)
$(call force,CFG_STM32_EXTI,y)
$(call force,CFG_STM32_GPIO,y)
$(call force,CFG_STM32_HSE_MONITORING,y)
$(call force,CFG_STM32_VREFBUF,y)
$(call force,CFG_STM32MP_CLK_CORE,y)
$(call force,CFG_STM32MP1_OPTEE_IN_SYSRAM,n)
$(call force,CFG_STM32MP1_SHARED_RESOURCES,n)
$(call force,CFG_STM32MP1_RSTCTRL,y)
$(call force,CFG_STM32MP13_CLK,y)
$(call force,CFG_STM32MP13_REGULATOR_IOD,y)
$(call force,CFG_TEE_CORE_NB_CORE,1)
$(call force,CFG_WITH_NSEC_GPIOS,n)
CFG_STM32MP_OPP_COUNT ?= 3
CFG_STM32_ADC ?= y
CFG_WITH_PAGER ?= n
CFG_WITH_TUI ?= y
endif # CFG_STM32MP13

ifeq ($(CFG_STM32MP15),y)
$(call force,CFG_BOOT_SECONDARY_REQUEST,y)
$(call force,CFG_DRIVERS_CLK_FIXED,y)
$(call force,CFG_DDR_LOWPOWER,y)
$(call force,CFG_HALT_CORES_ON_PANIC_SGI,15)
$(call force,CFG_SCMI_MSG_PERF_DOMAIN,n)
$(call force,CFG_SECONDARY_INIT_CNTFRQ,y)
$(call force,CFG_STM32MP1_SHARED_RESOURCES,y)
$(call force,CFG_STM32_PKA,n)
$(call force,CFG_STM32_SAES,n)
$(call force,CFG_STM32MP1_RSTCTRL,y)
$(call force,CFG_STM32MP15_CLK,y)
$(call force,CFG_STM32MP_CLK_CORE,y)
CFG_CORE_RESERVED_SHM ?= n
CFG_HALT_CORES_ON_PANIC ?= y
CFG_TEE_CORE_NB_CORE ?= 2
CFG_STM32MP1_OPTEE_IN_SYSRAM ?= n
ifeq ($(CFG_STM32MP1_OPTEE_IN_SYSRAM),y)
$(call force,CFG_WITH_PAGER,y)
CFG_STM32MP15_HUK ?= y
endif
endif # CFG_STM32MP15