Skip to main content
Associate II
March 4, 2025
Question

STM32MP135D-ODYSSEY - CRC check failed on FWU metadata with SD Card

  • March 4, 2025
  • 1 reply
  • 615 views

Hi, I was boot STM32MP135D-ODYSSEY with SD as boot option,using https://wiki.st.com/stm32mpu/wiki/STM32MPU_Distribution_Package and added odyssey dts. facing CRC check failed on FWU metadata and ERROR: loading of Bkup-FWU-Metadata failed. Can you help me with this.  ---- 

~$ sudo picocom -b 115200 /dev/ttyACM0
picocom v3.1

port is : /dev/ttyACM0
flowcontrol : none
baudrate is : 115200
parity is : none
databits are : 8
stopbits are : 1
escape is : C-a
local echo is : no
noinit is : no
noreset is : no
hangup is : no
nolock is : no
send_cmd is : sz -vv
receive_cmd is : rz -vv -E
imap is :
omap is :
emap is : crcrlf,delbs,
logfile is : none
initstring : none
exit_after is : not set
exit is : no

Type [C-a] [C-h] to see available commands
Terminal ready
NOTICE: CPU: STM32MP135D Rev.Y
NOTICE: Model: Seeed STM32MP135D Odyssey Board
INFO: PMIC version = 0x21
INFO: Reset reason (0x35):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe0000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r1.0(debug):38df888b0(38df888b)
NOTICE: BL2: Built : 01:36:41, Mar 15 2024
WARNING: CRC check failed on FWU metadata
WARNING: loading of FWU-Metadata failed, using Bkup-FWU-Metadata
WARNING: CRC check failed on FWU metadata
ERROR: loading of Bkup-FWU-Metadata failed
PANIC at PC : 0x2ffe524f

Exception mode=0x00000016 at: 0x2ffe524f

Screenshot from 2025-03-04 13-11-17.png

1 reply

Olivier GALLIEN
Technical Moderator
March 5, 2025

Hi @aravindhan ,

Could it be similar to Solved: STM32MP157F-DK2 failing to boot on custom image - STMicroelectronics Community ? 

Olivier 

 

 

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
March 5, 2025

Hi, thanks for the reply. Here Solved: STM32MP157F-DK2 failing to boot on custom image - STMicroelectronics Community he missed to add metadata.bin file, but I have added the file. Here is my Partition table:

Number Start (sector) End (sector) Size Code Name
1 34 545 256.0 KiB 8301 fsbl1
2 546 1057 256.0 KiB 8301 fsbl2
3 1058 1569 256.0 KiB FFFF metadata1
4 1570 2081 256.0 KiB FFFF metadata2
5 2082 10273 4.0 MiB FFFF fip-a
6 10274 18465 4.0 MiB FFFF fip-b
7 18466 19489 512.0 KiB FFFF u-boot-env
8 19490 150561 64.0 MiB 8300 bootfs
9 150562 183329 16.0 MiB 8300 vendorfs
10 183330 8571937 4.0 GiB 8300 rootfs
11 8571938 10485726 934.5 MiB 8300 userfs