Skip to main content
Associate II
June 30, 2024
Solved

STM32MP157 and LPDDR3 unused MPU pin consideration

  • June 30, 2024
  • 1 reply
  • 1112 views

Hello,

I designed custom board with STM32MP157 and LPDDR3 memory. Due to PCB manufacture restrictions I needed to connect to ground unused signal called DDR_ATO. I want to know if this is a problem, because if it is the case I can just remove 1 ball from the IC and solder it like that, but maybe it is not necessary?

 

Thank you, Dominik.

Best answer by PatrickF

HI @Badzonor 

We did not recommend to connect VSS to DDR_ATO ball.

DDR_ATO pin should be left open or connected to a test point.

Nevertheless, as a temporary workaround to start playing with your board, and until PCB is fixed, you could probably do it as it is mention that the pin will output '0' when not enabled.

PatrickF_0-1719840623860.png

 

Regards

1 reply

PatrickF
PatrickFBest answer
Technical Moderator
July 1, 2024

HI @Badzonor 

We did not recommend to connect VSS to DDR_ATO ball.

DDR_ATO pin should be left open or connected to a test point.

Nevertheless, as a temporary workaround to start playing with your board, and until PCB is fixed, you could probably do it as it is mention that the pin will output '0' when not enabled.

PatrickF_0-1719840623860.png

 

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here